On the Event Handlers form, use this drop-down list to determine the order in which custom event handlers execute for a given event, in cases where event handlers already exist for that event.
On the Event Handler Sequence form, this field is display-only.
If you have a handler selected in the Keep With drop-down list, you must also select an option in this drop-down list. If no handler is selected in the Keep With field, this field is optional.
You can use these two drop-down lists to modify the default handler sequence order. For more information and examples, see "About Event Handling and Order" in the Guide to the Application Event System.
This drop-down list displays a variable number of options, depending on whether or not you have a handler selected in the Keep With drop-down list. The following table lists and describes the possible options.
| Option | Description/Availability |
|---|---|
| (Blank) | If you select something in the Keep With field, you cannot leave this field blank. |
| First | This option causes your handler to execute first, before any others. |
| Before | This option causes your handler to execute before the handler selected in the Keep With field. |
| Instead | This option causes your handler to execute instead of
the handler selected in the Keep With field. When this
option is selected, the handler selected in the Keep With
field does not execute at all.
For possible exceptions to this rule, see "Overriding Others' Handlers" in the Guide to the Application Event System. |
| Exclusively Instead | This option is similar to the Instead option. The difference
is that, if this option is selected, it overrides all other
handlers, even those that use the Instead option with the
same handler.
For more information about this option, see "Overriding Others' Handlers" in the Guide to the Application Event System. |
| After | This option causes your handler to execute after the handler selected in the Keep With field. |
| Last | This option causes your handler to execute last, after all other handlers have finished. |