On the Event Handlers form, use this drop-down list in conjunction with the Chronology drop-down list to determine the order in which custom event handlers execute for a given event, in cases where event handlers already exist for that event.
You can use these drop-down lists to modify the default handler sequence order. For more information and examples, see "About Event Handling and Order" in the Guide to the Application Event System.
This drop-down list displays the event handlers associated with the designated event, by handler sequence number. To associate your event handler with one of these, select the handler sequence number.
NOTE: Your own handlers do not display in this list, because you cannot use this option in conjunction with your own event handlers, only those of others (as identified by the Access As identifier). To change the sequence of your own handlers, use the Event Handler Sequence form.
The Chronology drop-down list presents options for the order in which your event handler should be executed, in relationship to the handler sequence number selected here. For more information, see Chronology.
On the Event Handler Sequence form, this field is display-only.