Use the Intranets form to define intranets for this application. The intranets represent logical groupings of sites in your enterprise. An intranet can represent a grouping of application sites that exist together on a high-speed network, and for which you want common administration. Common administration can include replication, or creation of master sites.
An intranet can also represent an external application not built on Mongoose . This allows you to set up replication rules between this application's sites and external systems.
After defining your intranets, use the Sites/Entities form to define this application's database sites and assign them to an intranet.
For example, if you have two sites in one data center and two sites on a different data center, define two intranets, one for each data center, and put the sites from each data center on those intranets.
You cannot delete an existing intranet definition if either of the following statements is true:
Use the FAX fields on the Reports/TaskMan tab to set up faxing of reports to customers or vendors, for the reports supported by the Customer Document Profile and Vendor Document Profile forms. See Sending Reports to Customers or Vendors.
Use the SMTP fields on the Reports/TaskMan tab to set up sending of e-mail from TaskMan or the Application Event System.
Configuring Infor Framework Fax Service
Configuring a Third-Party Fax Service
Setting Fax Properties for a Specific Report or User