We recommend the default settings for synchronization because many customizations are merged automatically, which reduces editing time afterwards. This topic describes the default synchronization process.
In analyzing a customized form, Form Sync makes a three-way comparison between these three versions:
During analysis, Form Sync looks at component attributes, such as a component's data source or type, and form attributes, such as a form's caption or script.
If the base-level version of an attribute in the Source is:
Form Sync then replaces base-level versions of forms in the Target with base-level versions from the Source.
A global object is treated as a unit in synchronization—unlike a form, whose multiple specifications for component attributes and form attributes are handled individually in the merge process. The only options for handling a customized global object are to:
If the base-level version of a global object in the Source is:
Form Sync then replaces base-level versions of global objects in the Target with base-level versions from the Source.
When synchronizing the Explorer:
Because the All Forms folder is dynamically created from the forms database, the system automatically reflects any new base-level forms from the Source database.
Synchronizing with the Default Settings
Understanding WinStudio Customizations
Form Sync form