Synchronizing with the Default Settings
When you use the default settings to synchronize, the process affects
all customizations to all forms, all global objects, and the Explorer
in the Target configuration. For a description of the process and its
results, see About
Default Synchronization.
CAUTION: Before
synchronization, be careful to back up the forms database in the Target
configuration and confirm your database and server settings. For more
information, see Before
You Use FormSync.
To synchronize with the default settings:
- With the Form Sync form
open to the main page, click the Restore
Defaults button to ensure that all options are
set to their defaults.
- From the Synchronization base
level drop-down list, specify whether you want to synchronize
objects at the Vendor, Site, or Group
level.
For more information, see Synchronization
base level.
- Verify that the Only process objects
changed at the synchronization base level and the Process
scripts as single objects options are both selected.
- From the Log detail drop-down list, select the level
of detail you want to record in the log.
For more information, see Log
Detail Levels.
- On the Forms
tab, verify that the Merge
customized forms with base-level forms option is selected.
- Click Synchronize.
Form Sync proceeds with the synchronization process, using the default
settings.
Related Topics
About Synchronization
About Default
Synchronization