Displaying DataView Results

DataView results can be displayed in three ways:

Data

The DataView Results form and DataView Form Results form show data based on the properties that have been set on the DataViews Setup form and the DataView IDO Setup form. Properties differ by DataView and layout.

Options

You can specify this information on the DataView Results form:

Layout

If permissions are granted, you can save the current layout as the default layout or under a new layout name. You can delete and select existing layouts.

Display

Use these options to manipulate the data in the results grid:

Print

This menu provides standard print options.

Send To

Use this menu to send the data to a XPS or Excel .xls file.

Refresh

When available, use this option to reload the results grid, as if you had closed and reopened it.

Setup

When available, use this option to launch the DataViews Setup form pre-filtered to the current DataView.

Notes

If you do not have permission to see the results, an authorization message is displayed instead of the results.

If you cannot view costs, and cost properties are included in the DataView layout, then no data is displayed. In this scenario, we recommend that you copy the DataView to a new name, and deselect the cost properties.


Related Topics

About DataViews

Creating an Event to Call DataView Results