Setting Up DataViews

Use the DataViews Setup form to maintain DataViews, select the IDOs to use when results are displayed to the user, designate user and group permissions, and select data layout options.

Setting Up New DataViews

To set up a new DataView:

  1. On the DataViews Setup form, turn off Filter-in-Place.
  2. Click in the DataView grid, then select Actions > New to create a new DataView.
  3. In the DataView field, specify a name that best describes the data to be presented.
  4. On the General tab, specify this information:
  5. Click Save.

NOTE: This application is prepackaged with multiple DataViews. Prepackaged DataViews cannot be directly modified, but they can be copied to a new DataView name and altered.

Creating a DataView from an Existing DataView

To create a DataView from an existing one:

  1. Click Copy DataView to launch the DataViews Copy form
  2. Copy the default values from the currently selected DataView.
  3. Specify a new name for the DataView.
  4. Click Save.

Setting Additional Information for the DataView

Use the tabs to set additional information:

  1. On the User Permissions tab, specify this information:
  2. On the Layouts tab, specify this information:

Other Actions

Click Launch to execute the DataView, and open the DataView Results form for the currently selected DataView.

Click Import/Export to launch the DataViews Import/Export form, filtered for the selected DataView.


Related Topics

About DataViews

Setting Up an IDO for a DataView