The Window menu includes options for working with windows when you have multiple forms open. These options affect only form windows, and not the system windows, such as the Explorer, Settings, and Diagnostics windows.
NOTE: The web client has no Window menu.
| Menu item | Action |
| Cascade | Arranges all open form windows in a typical cascade arrangement. |
| Tile | Arranges all open form windows in a tiled arrangement.
The system attempts to space all windows evenly, first horizontally, then vertically. |
| Close All | Closes all form windows, including those that are minimized.
The system prompts you to save or cancel any changed data. If a form is open to find, add, or filter records into a parent form, the system gives you the option to return values to the parent form or not to return them. |
| Open form list | At the bottom of this menu, the system displays a list of all
the forms currently open, in the order in which they were opened.
The current active form (that has the focus) has a check mark
in front of it.
You can use this list to quickly select the form you want. |