The View menu includes a number of options for showing or hiding various elements of the user interface.
| Menu item | Action | Keyboard shortcut |
Explorer |
Opens and closes the Explorer window, which is used to access forms. For more information, see Using the Explorer. Not available in the web client. |
n/a |
User Preferences |
Opens the User Preferences window.
NOTE: You cannot use this option to close the User Preferences display.
To close the User Preferences
window, you must use the Close (x) button in the upper-right
corner of the main workspace.
This is where you can set your own user preferences. This window also includes options for setting editing and diagnostics preferences. For more information, see Setting User Preferences in the WinStudio Client or Setting User Preferences in a Web Client. |
n/a |
Inbox |
If the Inbox form is not open, this option opens it. If the form is open, this option brings it to the top and refreshes the display. This menu option generates a standard event, StdAppLaunchInbox. Developer users can generate or intercept this event. Not available in the web client. |
n/a |
Tasks |
If the Create User Task form is not open, this option opens it. If the form is open, this option brings it to the top. This menu option generates a standard event, StdAppLaunchTask. Developer users can generate or intercept this event. Not available in the web client. |
n/a |
System Notes |
Opens the System User Notes form, which allows you to create, read, and maintain reusable notes. For more information, see Working with Notes. Not available in the web client. |
n/a |
Toolbox |
Active only in Design Mode. When selected, displays the Toolbox for components in Design Mode. The Toolbox displays in a panel on the left side of the workspace, in the same space as the Object Viewer, if displayed. For more information, see About the Toolbox. |
n/a |
Object Viewer |
Active only in Design Mode. When selected, displays the Object Viewer in Design Mode. The Object Viewer displays in a panel on the left side of the workspace, in the same space as the Toolbox, if displayed. For more information, see Using the Object Viewer. |
n/a |
Form Properties |
Active only in Design Mode. When selected, indicates that the Form Properties sheet is displayed. This and the other properties sheets display in a panel on the right side of the workspace. |
n/a |
Component Properties |
Active only in Design Mode. When selected, indicates that the Component Properties sheet is displayed. This and the other properties sheets display in a panel on the right side of the workspace. |
n/a |
Object Properties |
Active only in Design Mode. When selected, indicates that the Object Properties sheet is displayed. This and the other properties sheets display in a panel on the right side of the workspace. |
n/a |
Diagnostics |
Opens and closes the Diagnostics window, which is used for debugging and other analytic tasks. Not available in the web client. |
n/a |
Status Bar |
Shows or hides the status bar. The messages on the status bar display information about your current actions. For example, if the form you opened has a note, the status bar displays NOTES. Not available in the web client. |
n/a |
Toolbar |
Shows or hides the main toolbar. Not available in the web client. |
n/a |
Activate Next Collection |
In forms that display multiple collections, this option moves the focus from one collection to the next. Not available in the web client. |
CTRL+F8 |
Home Cursor |
In a grid, moves the cursor to the first active column in the record (in which you can make a change). In a detail view or other type of form, moves the cursor (and the focus) to the first active field in the form. Not available in the web client. |
CTRL+HOME |
Default Size |
Active only in Design Mode. To set the current size of a form in Design Mode as the default size for any new forms to be created, click this option. Not available in the web client. |
n/a |
Hide/Show 1st Splitter Pane |
Toggles the grid view on/off. This option works only with multiview forms, query forms, or other forms in which there are both grid views and detail views. |
Ctrl+Shift+1 Does not work in the web client |
Hide/Show 2nd Splitter Pane |
Toggles the detail view on/off. This option works only with multiview forms, query forms, or other forms in which there are both grid views and detail views. |
Ctrl+Shift+2 Does not work in the web client |
Activate Next Pane |
Moves the focus from wherever the pointer currently is to the other pane. This option works only with multiview forms, query forms, or other forms in which there are both grid views and detail views. Not available in the web client. |
F6 |
Warnings |
Opens the Warning Messages dialog box, which allows you to view active warning messages for a form and correct problems before saving and closing the form. Not available in the web client. |
n/a |
Explorer Editor |
When selected, displays the Explorer Editor, which is a read-only display of the Mongoose Explorer. Available only in the web client. |
n/a |