Design Time settings control aspects of how forms look and behave when you are in Design Mode. You need these only if you are actively involved with creating or modifying forms in the system.
To make design time settings:
Adjust the settings to your preferences.
For details about the settings on this tab, see these tables:
| Setting | Comments |
Development Mode |
This option controls how properties display in the Form and Component property sheets:
|
Show Hidden Components |
When selected, hidden components on a form are displayed when you are in design mode. When cleared, components remain hidden. |
Enforce Strict Locking of Forms and Objects |
NOTE: This option applies
only to those who have editing permissions of Site Developer
or vendor developer.
When selected, this option causes the system to:
We recommend that this option be selected in any environment where there are multiple developers designing and/or modifying forms. |
| Guidelines | Enter the width and height values in "character units"
that you want to use for the grid.
These settings control:
|
| Setting | Comments |
WinStudio |
WinStudio has a built-in script editor you can use to develop scripts. To use this built-in script editor, select this option. This script editor is a very basic editor. If you plan to do any extensive form development and/or customization, we recommend that you use one of the Visual Studio options. |
Visual Studio 2010 |
If you have Microsoft Visual Studio 2010 installed on your computer and you prefer to use that (instead of the built-in script editor) to develop scripts, select this option. NOTE: Infor neither provides nor installs Visual Studio 2010 as part of its software. You can select this option only if you already have Visual Studio 2010 installed on the same computer that you are using to develop scripts. |
Visual Studio Express VB Visual Studio Express C# |
If you have Visual Studio 2010 Express installed on your computer and you prefer to use that (instead of the built-in script editor) to develop scripts, select one of these options. You can specify whether you prefer to script in Visual Basic (VB) or C#. Attaching the Visual Studio debugger to an external application such as WinStudio.exe to initiate an interactive debugging is not supported in the Visual Studio Express editions; it is supported for the full Standard, Professional, or Team editions of Visual Studio. When you open the EditWinStudioScript project in Visual Studio Express from WinStudio, the script code class (ScriptClass.vb) is not automatically opened. You must open the ScriptClass.vb file from the Solution Explorer to edit the script. NOTE: Infor neither provides nor installs Visual Studio 2010 Express as part of its software. You can select this option only if you already have Visual Studio 2010 Express installed on the same computer that you are using to develop scripts. |
| Setting | Comments |
Visual Studio Modeless |
This option is enabled only if you select the Visual Studio 2010 option. In most cases, you should leave this check box selected. This minimizes the Edit Script in Visual Studio dialog box and makes it modeless; that is, as soon as you click Save in the Visual Studio IDE, the changes to your script are copied to the WinStudio cache and marked as modified. In addition, you can exit WinStudio Design Mode and still access the Visual Studio instance from Runtime Mode. For more information, see Edit or Create a Script with Visual Studio. Enable the modal interface (that is, clear this check box) if you want to enforce modal dialog access to Visual Studio. In this case, you can only edit scripts while you are in Design Mode. |
Path to Visual Studio Express Application |
This option is enabled only if you select one of the Visual Studio Express options. To instruct WinStudio where to find the Visual Studio Express application executable (.exe) file, click Browse. If you have selected one of the Visual Studio Express options, and you enter an incorrect path here or leave this field blank, an error displays when you leave this field. |
Edit or Create a Script with Visual Studio