Like the WinStudio smart client, you can set a variety of display and operational preferences. The options you have in a web client, however, are more limited than in the smart client.
The web client offers these user preference options:
| Option | Notes/Description |
Wildcard character |
Enter the character to be used as a wildcard character when you search for information with Filter-in-Place or query forms. The default character is the asterisk (*). |
Show configuration name on caption |
When selected, this option causes the name of the system configuration to which you are currently logged on to display in the title bar of WinStudio. |
Auto-delete all unmodified new rows |
Under normal system operation (that is, when this option is not selected), any row that the system inserts in a grid automatically is automatically deleted if you move away from the row without changing anything in it. However, the system does not treat rows that you create using a menu option, toolbar option, or keyboard shortcut the same way. With these rows, the system normally attempts to validate them, whether you have modified them or not. When this option is selected, the system treats all new rows as if they were inserted automatically by the system. In other words, if you manually create a row and then navigate away without changing anything, the system automatically deletes it. |
Prompt to save form splitter changes |
When selected, this option allows you to save any changes you might have made to the position of the splitter bar in multiview forms. For example, suppose you have a multiview form open, and at some point, you moved the splitter bar to enlarge your view of the grid side of the form. You like that change and want to make it permanent, so that every time you open the form, the splitter bar is right where you positioned it. If this option is selected, when you try to close the form, the system displays a confirmation box that asks if you want to save the current splitter bar position. To save the form configuration, click Yes. If this check box is cleared, you cannot save splitter bar position changes at all. |
Prompt to save grid changes |
When selected, this option allows you to save any changes you might have made to the grid view in multiview forms. For example, suppose you have a multiview form open, and at some point, you widened some columns and narrowed other columns on the grid side of the form. You like the changes and want to make them permanent, so that every time you open the form, the grid side is just as you have it now. If this option is selected, when you try to close the form, the system displays a confirmation box that asks if you want to save the current grid side configuration. To save the configuration, click Yes. If this check box is cleared, you cannot save grid side changes at all. |
Data Record Cap |
The term caps refers to the maximum number of records or items that the system can return at one time. There are two types of caps that you can reset for your work:
Both of these types of caps have the same three options:
This setting is not saved when you sign out of the system. NOTES:
For more information on caps, see About Caps. |
Language |
From the drop-down list, you can select a language for the text in field labels, button labels, menus, online help, and other parts of the user interface. Then click Apply. When you click Apply, the User Preferences window closes. NOTE: Only those languages that are installed and available on your system appear on this drop-down list. |
The web client offers only one layout option: Theme
Use the drop-down list to select a theme. Any user-created themes will be shown here along with two that are provided with the application. The two options that are provided by default are:
NOTE: The web client honors only the settings for background colors, foreground colors, and fonts for any given theme. The web client does not honor settings for non-tabbed form layout, menu bar, group boxes, notebook tabs, or the Explorer.
For more information about themes, see About Themes.
The web client offers only one Event System option: Handler editing mode
This option has to do with the display of metadata in the Event Actions form and with the behavior of the Event Handler Diagram form. You can choose to interact with these forms either in Normal mode or in Expert mode.
For more information, see Handler Editing Options.
Setting User Preferences in the WinStudio Client