About Incident Escalation
Use incident escalations to notify designated people, based on criteria
you define, when an incident reaches its follow-up date, warning date,
or late date. The follow-up, warning and late dates for an incident
are determined by to the priority code that is assigned to each incident.
Automatic notification of incidents is handled through a "watchdog"
utility that you can place on the background queue. This Escalation
Utility monitors the system and automatically performs escalation
actions.
Setup
Use these steps to set up incident escalation:
- Define the weekly billing
hours on the Contract tab of the Service
Parameters
form. These fields work in conjunction with the Coverage
fields on the Service
Priority Codes
form.
- Define a Supervisor on the Partners
form. This field applies only if using the escalation task requires
a supervisor.
- Use the Incident
Escalation Tasks form to set
up escalation activities by priority code. (You define when, how,
and to whom notifications will be sent. (The basis for the follow-up,
late or warnings are defined on the Service Priority
Codes form.) On the Incident
Escalation Tasks form, you can set notification options
such as these:
| Option |
Description |
| E-mail |
Send an e-mail to the incident owner, supervisor, SSR,
contact, etc. |
| Status Change |
Change the incident status code value. |
| Priority Change |
Change the incident priority code value. |
| Text Message |
Send a message to a text message service. |
| Create Event |
Create an event to record the escalation occurrence/ |
| Owner Change |
Change the incident owner value. |
- On the Service Parameters
form, assign a default priority code to use for all incidents. On
the Service
Customers, Units, or Service Contracts
forms, assign priority code default values to specific customers,
units or contracts, as needed. (A priority level default can also
be set for items and service types, to simplify the setting up of
units and contracts.)
Built-in Escalation (How Default Priority Codes Are Determined)
When you create an incident, the priority code assigned to the incident
defaults from the values set at other levels, using this hierarchy:
- If the unit on the incident is populated, and that unit is under
an active contract, use the contract priority code, if not blank.
- If the item and customer on the incident are populated and that
item/customer combination is under an active contract, use the contract
priority code, if not blank.
- If the customer on the incident is populated and that customer
has an active contract, use the contract priority code, if not blank.
- If the unit on the incident is populated but not found on an active
contract, use the unit's priority code, if not blank.
- If the item on the incident is populated but not found on an active
contract, use the item's priority code.
- If the customer on the incident is populated but not found on an
active contract, use the customer's priority code,if not blank.
- If no other level in this hierarchy has a priority code defined,
use the default priority code from the Service
Parameters form.
When you save the incident record, the Escalation Tasks tab on the Incidents form displays the escalation
tasks that are automatically associated with the incident. Escalation
tasks which have rules which do not match that of the incident are displayed
but marked as inactive.
You can change the escalation tasks or add new tasks that are created
specifically for this incident.
Running the Escalation Utility
Run the Incident
Escalation Utility, which determines what escalations should
be performed. The utility can be run at set intervals on the background
queue.
The utility performs these functions:
- Reviews all active escalation tasks for each open incident.
- Compares the current date to the date of the escalation basis.
- Determines the escalation frequency.
- Performs the escalation action.
- Creates an escalation log entry.
- Sets the Last Processed Date for each affected incident.
How an incident is escalated is determined by the priority of the incident,
but what triggers the escalation can be based on criteria you set for
Due Date, Follow-up, Late or Warning time lines. In addition, you can
determine how often the escalation notification can occur - for example,
once, hourly, or daily.
Viewing the Incident Escalation Logs
The Incident
Escalation Logs form keeps track of the escalation tasks that
were processed for each incident.
Related Topics
Setting Up Escalation
Tasks
Setting Up
Service Priority Codes