Setting Up Priority Codes that Establish Response Times for Incidents

On the Service Priority Codes form, specify this information to set up codes that describe incident priorities, for example High, Low, Medium, and Urgent.

To set up a new code:

  1. Specify this information:

    Priority Code

    Specify a code that defines the urgency of the incident. The default priority code value that will be used in incidents is set in the Service Parameters form. See also the section on "How Default Priority Codes are Determined" in About Incident Escalation.

    Description

    Specify a description that explains the priority code.

    Days Until

    Use these fields to establish default response times for an incident of a certain priority. For example, a "Medium" priority can be configured to warn after 7 days, be late after 15 days, and prompt for follow up after 30 days, and a "High" priority can follow up within 8 hours, warn after 2 days, and be late after 3 days.  Provide values in the Hours fields if the elapsed time must be less than a day. The values you set on this form are used, along with the date of the incident, to calculate default followup, late, and warning dates in the Incidents form when you specify a priority for an incident. You can manually override them, but if you later change the incident's priority, the default values for the new priority code override your manually entered values.

    Coverage Basis

    Specify the hours to consider as part of the "Days/hours until..." value when the system sets warning, due, and follow-up dates for incidents:

    Note: The Service Holidays option on the Service Parameters form determines whether holidays entered in the back office application are included or excluded from the priority date calculation for Business Hours and Contract Coverage Hours. All Hours means all, regardless of holidays.

  2. Save the record.

Escalation Tasks

Click Escalation Tasks to open the Escalation Tasks form, where you can set up escalation activities for each priority code. After you set up the tasks there, they are displayed in the grid on the Service Priority Codes form.


Related Topics

Setting up the System for Incidents

About Incident Escalation