Approving Partner Expenses

Use the Expense Approval form to approve material, labor, and miscellaneous transactions entered by a partner. Partner transactions must be approved prior to reimbursement or reconciliation.

To approve an expense:

  1. Specify this information on the form:

    Bill Manager

    Select the partner identification of the person responsible for verifying that the SRO is properly invoiced.

    Partner

    Select the partner associated to the SRO.

    SRO

    Select the SRO associated to the expense.

    Line

    Select the SRO line associated to the expense.

    Operation

    Select the SRO operation associated to the expense.

    Reimbursement Status

    Select the status of the transaction:

  2. These values are displayed:
  3. Click Refresh to populate the grids with the applicable transactions.
  4. Select individual transactions in each grid or click Select All to select all the transactions for approval.
  5. Click Approve to process the approval.

Buttons

Use these buttons on the form:


Related Topics

Reimbursing Partner Expenses