Use the Service Order Automatic Generation Utility to process the specified units and automatically generate a SRO if needed.
When Auto Schedule Resource is selected on the Service Parameters form, then an appointment is created for each maintenance SRO. These values are used to create the appointment:
Partner
Appointment Date:
Duration
To automatically generate a service order:
Unit
Select the range of units to include for the utility.
SRO Type
Select the range of SRO types to include for the utility.
Dept
Select the range of departments to include for the utility.
Work Center
Select the range of work centers to include for the utility.
Through Date
Specify the date through which the SROs should be automatically generated.
Select this field to automatically increment date ranges.
Keep Operation Numbers
Select this check box to use operation numbers as they appear on the SRO template. If not selected, the numbers are re-sequenced in increments of ten.
Using SROs to Track Service Requests, Transactions, and Billing