Copying Inspections

Use the Inspections Setup Copy form if you want to add a new inspection setup that is similar to an existing one. Follow these steps to copy an inspection:

  1. Launch the Inspections Setup Copy form.
  2. In the From section, select the item, inspection type, and section code that you want to copy.
  3. In the To section, select the item, inspection type, and section code for the new inspection.
  4. Click OK to complete the copy.

To stop the process, click Cancel.


Related Topics

About Inspections

Setting Up Inspections