Service Order Quick Create: Copying SRO Information from an Existing SRO

You can quickly specify a simple list of information to create a Service Request Order or copy it from an existing SRO or template. The system then builds the SRO structure from the specified template, unit, and customer.

Use the Service Order Quick Create form, accessed from a button on the Service Orders or Service Console forms, to do this.

Quickly Creating a Simple SRO

On the "Copy To" side of the Service Order Quick Create form, just specify the Customer Number, Ship To, and Unit Substitute fields to quickly create an SRO structure. Then click OK to display the new SRO in the Service Orders form.

Copying an SRO To/From an Existing SRO or Template

  1. Specify this information about the SRO or template you are copying from, in the Copy From area of the form:

    Copy From SRO

    Select the SRO you want to copy to make the new SRO.

    Only Show Templates

    Select this check box to limit the selections available to only include SRO templates.

    Keep Line Numbers

    Select this check box to create the line numbers as they appear on the SRO from which they are copied. The line numbers will not be re-sequenced. Clear this check box to re-sequence the line numbers, starting with the number one and incrementing by one.

    Keep Operation Numbers

    When the maintenance is set up on the Units form, a SRO Template is selected for creating the service order. Select this check box to use the operation numbers as they appear on the SRO Template. Clear this check box to re-sequence the numbers to the standard operation sequencing of 10, 20, 30, and so on.

    Use SRO Whse

    Select this check box to assign the value from the new service order (General tab, Warehouse field) to the operation(s) and any transaction(s) being copied. This replaces the warehouse value as it was set on the original operation or transaction. If this check box is cleared, then the warehouse value of the operation and transaction keeps the value from the original SRO.

    Auto Schedule Resource

    Select this check box to automatically create an appointment for the SRO. The appointment is displayed in the grid section of the Schedules tab on the Service Orders form when this functionality is enabled.

    Available Operations Grid

    This grid shows the operations associated with the selected SRO that are available for inclusion in the copy or creation utility. Use the arrow buttons for moving operations between this area and the Operations to Include area.

    Copy Transactions From

    Select which transactions to copy from the selected SRO operations. Valid options are:

    Copy Line Transactions

    Select this check box to copy the line transactions.

  2. Use the arrow buttons to move specific lines or operations back and forth between the "From" area to the "To" area.

    NOTE: When you copy across database sites, all lines and operations are copied. You cannot select specific lines or operations.

  3. Specify this information about the SRO you are copying to, in the Copy To area of the form:

    Customer

    Select a customer for the new SRO.

    Ship To

    Select a customer ship to location. If the field is left blank, the zero ship to location is the default value.

    Start Date

    The date specified is assigned to the SRO and Operation Start Date/Time. If the Automatic Resource Scheduling functionality is turned on, this value is also used as the start date/time of the scheduled appointment. The Start Date will default to the current system date and time, and will be pushed out by the lead time (if specified) of the SRO Type.

    Lead Partner

    Select the lead partner for the SRO.

    Unit Substitute

    Select a unit to replace the one being copied from the selected SRO Line.

    Item Substitute

    Select an item to replace the one being copied from the selected SRO Line.

    Qty

    Specify the number or amount of units/items to use on the transaction, order, etc.

    UM

    Select the unit of measure for the item.

    Show All Operations

    This check box works in conjunction with the item substitute fields on the form. If one of those fields is specified, the utility only shows operations that match the item selected. But if this check box is selected, then the matching functionality is overridden and all the operations from the selected SRO are displayed.

    Operations To Include Grid

    This grid shows the operations associated with the SRO that are available for inclusion in the copy or creation utility.

    Copy Transactions To

    Select which transaction type to create on the new service order. Valid options are:

    Comp Item Substitute

    Select an item to replace the item on the material transaction of the operation being copied from the existing SRO.

    Comp Qty

    Specify the number or amount of units/items to be used on transaction, order, etc.

  4. Click OK to save the changes and create the new SRO, or click Cancel to cancel the process.

Copying a Line from an Existing SRO

Click Copy Lines on the Service Orders form to open the Service Order Quick Create form and quickly copy a line from the displayed SRO to another SRO.


Related Topics

Automatic Resource Scheduling