Running the Indented Unit Configuration Report

Use the Indented Unit Configuration Report utility to generate a report output showing unit configuration and warranty information for the subcomponents of the unit. The report is time phased so the change in configuration over time can be displayed. Follow these steps to run the report:

  1. Open the Indented Unit Configuration Report.
  2. Specify this information:
  3. Include Warranty

    Select this check box to include the warranty information associated with the unit as part of the report output.

    Level

    Select the lowest level to be displayed in the indentation of the unit configuration. If the value is set to 0 then all levels are displayed.

    Page Break Between Units

    Select this check box if you want to have page breaks between units on the report.

    Starting/Ending Unit

    Select the range of units to include for the report.

    Starting/Ending Item

    Select the range of items to include in the report.

    As Of Config Date

    Indicate the last possible configuration date of a unit in order to qualify for this report. Any unit with a configuration date earlier than this value is included in the report. This field defaults to the current date.

  4. Click Preview to view an output of the report.
  5. Click Print to run the utility and print the report.

Related Topics

 About Items, Units, and Servicing