A partner is a resource (employee, customer, or vendor) who can resolve incidents or SROs. Partners can be specified as the SSR and/or as the "owner" of an incident. Partner IDs can be linked to employee IDs, customer IDs, vendor IDs, and/or user IDs.
Use the Partners form to specify information about your company's partners:
Partner
Specify an abbreviated version of the name of the partner.
Type
Select the category that a partner belongs to:
Ref Num
Select the partner reference number. This is the associated customer, employee, or vendor.
Ship To
Select the ship to location to associate with the partner. This field is enabled only for partners with the type Customer.
Name
Specify the name of the partner.
Active
Select this check box if the partner is currently active.
Supervisor
Select the supervisor of the partner.
Schedule Button
Click this button to launch the Service Scheduler.
Specify the email address.
Warehouse
Select the warehouse that a partner may issue inventory out of while working on a SRO.
Labor Cost
Specify the hourly cost for a partner.
Hourly Rate
Specify the hourly rate of a partner for the type of work being performed.
Default Misc Code
Select the unique alphanumeric code that represents a particular type of expense that is charged to a SRO. These codes can be used to ensure that the expenses are charged to the proper general ledger account. These codes are set up on the Miscellaneous Codes form.
Default Work Code
Select the code used to represent the type of work that is being recorded to a SRO. Codes are set up and maintained on the Work Codes form.
Default Payment Type
Specify the payment type to be used by default for miscellaneous SRO transactions that are submitted from the Reseller Portal. Available selections are set up and maintained on the Payment Types form.
Department
Select the department out of which the partner works.
User
Select a User ID from the list. The list is populated from the Users form.
Reimbursement Method
Select the method to be used or the type of payment to be included for partner reimbursements. Valid options are voucher, credit memo, other, and all.
Reimburse Material
Select this check box to reimburse the partner for material transactions on incidents that the partner is assigned to. If this field is not selected, costing is not affected for associated transactions.
Reimburse Labor
Select this check box to reimburse the partner for labor transactions on incidents that the partner is assigned to. If this field is cleared, costing for the associated transactions is not affected.
Currency
Select a default currency code to associate with the partner. This will be used for reimbursement currency conversion.
Weekly Available Hours
Specify the maximum block of time that a partner is to be scheduled for a task or tasks on any given day.
Display On Schedule Board
Select this check box to display the partner on the board within the Service Scheduling module.
Exchange Integration Enabled
This check box is selected if the Exchange Integration service is enabled for the user.
Exchange Folder
Optionally, specify a destination folder for the Exchange Integration service. In most cases, this field can be left blank and the appointments will be synchronized with the user’s default Inbox Calendar based on the email address setup in Exchange.
In the Last Known Location section of this tab:
Region
Select the region code for the partner.
Description
The description of the region is displayed.
Country
State
County
City
Postal Code
Partner
For partner records that are set up as a team, select the partners that make up the team.
NOTE: Partners can be members of more than one team.
Name
The partner name is displayed.
Team
Select any team(s) to which the partner belongs.
NOTE: A team record is set up in the same way as a partner record using the Partners form.
Name
The partner name is displayed.
Team Substitutions Button
Click this button to launch the Partner Substitutions form, filtered for the selected partner/team record and the current system date.
Refresh Skills Button
Click this button to delete all the skills currently associated with a team and rebuild the list by adding skills currently held by any partner on the team. The new skill set is stored on the Skills tab of the team record.
Refresh Certifications Button
Click this button to launch the SRO Quote form, linked for the current SRO.
Click the Schedules button to display the Service Schedules form, where you can see scheduled appointments related to service work.
Setting up the System for Incidents
Setting Up the System to Work with Exchange