Using the Call Center to Add and Track Incidents
This process flow describes the general steps used in adding an incident
and then tracking it through the system:

Recording the Initial Support Request
Your support representative (sometimes referred to as an SSR) receives
initial requests for service via phone call, fax, e-mail, etc. These requests
are recorded in the Incidents
form. The SSR first determines whether the customer is calling about an
existing incident, or whether a new incident must be created. If
a new incident must be created, the SSR records the information that is
needed to resolve the issue on the Incidents form:
- Customer information: Name, address, phone, fax, e-mail and any
other contact information.
- Unit information: The serial number and item of the part that needs
to be serviced. When a unit is identified, its warranty and contract
information is added to the incident.
- Reason codes: General and specific codes that identify the problem
and assist in routing the incident to the appropriate resources.
- Owner: the technician who is assigned to perform the service. Technicians
are usually assigned based on the type of unit, type of service, or
region.
- Incident priority/status: Record the severity of the incident,
along with the status. Priority codes can be used to establish expected
response times for "Follow up," "Warning," or
"Late" incidents. When priority codes are used with the
escalation feature, the system can alert you to potential issues.
- SRO cross-reference: If an incident requires service that must
be billed, you can cross-reference the incident to an SRO, using the
Destination Type.
If the call is about an existing incident, the SSR adds a new event on the Incidents
form to record the customer's inquiry about the incident. Any activity
related to the incident can be captured as an event. Events are
user-definable, typically with names such as CallIn, CallOut, EmailIn,
EmailOut, Dispatch, Notes, etc.
When an incident is resolved, specify the resolution, both general and
specific, for future reference.
Reports and Historical Information
These reports are available related to incidents:
Related Topics
About SyteLine Service
Adding an Initial Request for
Service (Incident)
Quick Incident
Creation
Incident Escalation