Order Shipping

The Order Shipping form allows you to enter shipping transactions and track shipped items by ship date. Before generating a regular invoice for an item or an order, you must ship that item or order. Once you ship an item, it will appear on the To Be Invoiced report.

NOTE: This functionality is different from the Picking, Packing, and Shipping functionality, and it is recommended that you either choose to use the picking, packing, and shipping functionality or use the standard shipping functionality (Order Shipping form). They were not designed to be used together. Even though the two are separate, there is some interaction. If you ship a quantity through Order Shipping or return a quantity through Order Shipping, the Pick Workbench is aware. If there is quantity in use through the Picking, Packing, and Shipping process, the Order Shipping form is aware.

The Detail tab shows information about the order line you selected.

The Customer Credit Return tab is enabled only if CR Return is selected for the active row in the grid.

The Actions menu includes these options:


Related Topics

Manually Shipping a Customer Order

About Cross-Referenced Blanket Releases and Order Shipping

Performing a Quick Return of an Entire Order

Processing Customer Returns After Invoicing

Processing Customer Returns Before Invoicing

Shipping an Order with Reserved Inventory

Using Utilities and Activities

About Credit Hold

Serial Numbers Tab/Area