About Cross-Referenced Blanket Releases and Order Shipping
This topic describes how the quantity to ship value
on the Order
Shipping form changes based on how a blanket line release is cross-referenced.
If Cross Referenced to a Job Order
If a blanket line/release is cross-referenced to a job when you complete,
post, and move a quantity from the job to inventory, the following occurs:
- The system uses the Job Quantity Moved to update the Ready
Quantity in Order Shipping for the cross-referenced line/release.
The system uses the quantity moved to inventory on the job as the
default quantity to ship on the Order Shipping form.
- If the line/release status is currently Planned, the system
changes the status to Ordered.
NOTE: If a line/release
is a planning
item, you cannot update the Config String for any line/releases
that have a cross reference.
If Cross Referenced to a Purchase Order
If a line/release is cross-referenced to a PO, the
following occurs when the PO is received:
- The system uses the Received value of the corresponding
purchase order (PO) line/release to update the CO Quantity Ready
for the cross-referenced CO line/release. The system uses the Quantity
Ready of the PO line/release as the quantity to be shipped on
the Order Shipping form. Returns against the cross-reference
reverse these figures.
- If the line/release status is currently Planned, the system
changes the status to Ordered.
Related Topics
Customer
Orders Overview
Cross-Referencing
Demands to Supplies
Cross-Referencing
a Customer Order to a Job Order
Customer
Order Blanket Lines
Order Shipping