Purchase Orders Quick Entry

CAUTION: The Purchase Orders Quick Entry form cannot be opened if, in the Use PO Change Order field on the Purchasing Parameters form, you have selected Sometimes or Always.

Use the Purchase Orders Quick Entry form to quickly create and maintain purchase orders and their associated lines. Once the request is made and approved, the purchase order can be used to authorize payment and ensure that the correct items are received.

When you delete a purchase order, all associated line/releases and notes for that line are also deleted.

Deleting a purchase order with a status of Ordered or Complete requires that the Order Qty, Qty Received, and Qty Rejected fields equal zero. If they do not equal zero, a message explains that the line may not be deleted and you will be returned to the form.

The Allocate Landed Costs activity is accessible from the Actions menu. You can also display lists of receipts, GRNs, and PO requisitions from the Actions menu.

NOTE: You cannot delete a PO that has any change orders with a status of Open or Final.

Actions Menu

On the Actions menu, you can choose List Change Log, List Receipts, List Goods Receiving Notes, and List Purchase Order Requisition Lines.


Related Topics

Purchasing Overview

Adding a Blanket Purchase Order Header

Adding a Regular Purchase Order Header

Changing a Purchase Order Header Status

Creating Multi-Site Purchase Orders with the Purchase Order Builder

Creating an EDI Purchase Order (Outbound 850/ORDERS)

Deleting a Purchase Order

Using Demand and Source Vendor Site PO-CO Automation

Change Status, Change Order/Purchase Orders

Creating and Approving a Purchase Order Requisition

Linking a Vendor LCR to Vendors and Purchase Orders

Purchase Order Blanket Lines

Purchase Order Blanket Releases

Purchase Order Lines