CRM Overview
CRM is a customer relationship management solution that provides an 
 efficient method for managing the entire sales process within SyteLine, from customer 
 lead origination and sales opportunity tracking through converting prospects 
 to customers and placing the order.
The features in CRM provide an integrated solution between your front 
 and back offices. It delivers productivity gains by streamlining sales 
 and customer service processes, decreasing the cost of sales and cost 
 to serve, and ultimately increasing revenue.
CRM allows you to manage your marketing, sales, order, contact, and 
 customer management activities:
	- Marketing - Using the Opportunities 
	 form, your marketing organization can track all elements of a marketing 
	 or sales campaign, including its effectiveness. You can also manage 
	 all tasks associated with an opportunity using the Opportunity 
	 Tasks form. Use the Competitors 
	 form to keep contact information and basic company information of 
	 your competitors. Create campaigns with the Campaigns 
	 form, and add items to the campaign with the Campaign 
	 Items form. Use the Campaign 
	 Types and Campaign 
	 Statuses forms to add further detail to your campaign.
 
	- Sales - Using the Prospects and 
	 Leads 
	 forms, your sales representatives can assist prospects and customers 
	 from initial interest through order placement. They can quickly convert 
	 a prospect to a customer. All associated information is automatically 
	 transferred to the new customer and opportunity records. They can 
	 also organize prospects and customers by Territories. 
	 Use the Sales 
	 Teams form to create and manage sales teams for customers, 
	 prospects, and opportunities. Use the Sales 
	 Contact Interactions form to keep track of communications 
	 with sales contacts. The Sales 
	 Contacts form allows you to keep basic information on your 
	 sales contacts. Use the Sales 
	 Forecasts form to keep track of sales forecasts and the Add 
	 Opportunities form to add opportunities to a sales forecast. 
	 Create sales periods with the Sales 
	 Periods form. The Prospect 
	 Interactions form and Customer 
	 Interactions forms allow you to keep track of communications 
	 with prospects and customers.
 
	- Order Management - The Opportunities 
	 form also allows you to track estimate orders assigned to prospects 
	 or customers.
 
	- Customer and Sales Contact Management 
	 - On the Customers 
	 form, CRM tab you can maintain territory information, the SIC code, 
	 company revenue and number of employees for each customer. You can 
	 also cross reference your sales contacts with customers 
	 and prospects.
 
Licensing
Any user with the SyteLineTrans 
 license module can access the CRM forms.
CRM Recommendations Including Order of Events
We recommend that you use CRM in a test environment first so that you 
 become familiar with how it works before using it in your live environment.
Order of events:
	- Identify the base values for the various fields on the CRM forms. 
	 Several of the CRM forms each have dropdown fields for which values 
	 need to be defined. Some are required, and some are optional. If possible, 
	 the dropdown values should be set up before importing CRM data or 
	 entering any data into these forms (with exception to the Customers 
	 form/table which most likely already has data). Those forms that have 
	 these dropdown values include: Leads, 
	 Opportunities, 
	 Opportunity 
	 Tasks, Prospects, 
	 and Customers. 
	 
	
When defining the values, it is important to think about how you 
	 will use CRM and how you want to track progress on leads and opportunities, 
	 as well as tracking other information such as where the lead or opportunity 
	 came from, what was the reason for the win or loss, and what types 
	 of tasks might there be when working with an opportunity. You also 
	 need to decide if you want to track your data by territory. Your Infor Business Partner or the 
	 Infor PSO team can assist with defining these values based on the 
	 needs of your organization.
	
		NOTE: Although the system won't 
		 prevent you from changing the values later, it may be undesirable 
		 as it would invalidate any existing records with those values. 
		 Scripts could be written though to update any existing records 
		 prior to changing the values. 
	
	The values that need to be defined include:
	
		- Lead Statuses (required - Leads form)
 
		- Opportunity Statuses (required - Opportunities form)
 
		- Opportunity Sources (optional - Leads and Opportunities 
		 forms)
 
		- Opportunity Stages (optional - Opportunities form)
 
		- Opportunity Won Reasons (optional - Opportunities form)
 
		- Opportunity Lost Reasons (optional - Opportunities form)
 
		- Opportunity Task Types (optional - Opportunity Tasks 
		 form)
 
		- Territories (optional - Customers and Prospects 
		 forms)
 
	
 
	- Enter/import your Sales 
	 Contacts. You can import contacts from Outlook or set them 
	 up manually. If you have the data defined in another database, you 
	 may want to create import scripts to import the data. We recommend 
	 you contact your Infor 
	 Business Partner or Infor PSO to assist with this process.
 
	- Set up any existing Prospects 
	 and then cross reference them to your Sales Contacts, using the Prospect 
	 Sales Contact Cross References form.
 
	- Cross reference any of your existing customers to the contacts 
	 you imported or manually set up. Use the Customer 
	 Sales Contact References form to complete this.
 
	- Enter any existing leads, opportunities, opportunity tasks, and 
	 quotes that you already have and want to begin tracking. If you need 
	 to import these, we recommend you contact your Infor 
	 Business Partner or Infor PSO to assist with this process.
 
	- Begin using CRM.
 
Technical Points
	- When importing/exporting sales contacts from/to Outlook, this is 
	 not a synchronization. Records are duplicated if they already exist 
	 (in either direction). So, if importing from Outlook, and the contact 
	 exists already in CRM, importing it again creates another sales contact 
	 record. If exporting to Outlook, if the contact exists already in 
	 Outlook, exporting it again creates another Outlook contact.
 
	- When importing/exporting sales contacts from/to Outlook, Outlook 
	 must be open. When importing, highlight all contacts in Outlook to 
	 be imported. Click the import button to bring over those selected 
	 contacts. When exporting, either the selected record in SyteLine or all records 
	 will be exported, depending on if you select the Export or Export 
	 All button.
 
	- The ability to assign territories is used for tracking purposes 
	 only, such as reporting. It does not limit users to only the data 
	 in their assigned territories (data is not filtered by territory).
 
	- You can create your own reports with CRM data or export the data 
	 to Excel. Your Infor 
	 Business Partner or the Infor PSO team can assist with creating reports 
	 if this is desired.
 
	- There are pre-defined query forms available under the CRM>Queries 
	 folder. These forms allow you to query your campaigns, competitors, 
	 sales contacts, sales teams, sales forecasts, prospects, leads, opportunities, 
	 and opportunity tasks based on the data of your choice.
 
	- You can generate events against the forms. This can be helpful 
	 for things such as managing the progress of opportunities and tasks, 
	 following-up on leads or opportunities, etc. For more information 
	 on the SyteLine 
	 Application Event System, see the Guide to the Application Event 
	 System on our support 
	 site. If needed, your Infor Business Partner or the Infor PSO 
	 team can assist with creating events to meet the needs of your company.
 
The following chart displays how the CRM components are related to each 
 other:

Related Topics
Creating and 
 Managing Opportunities
CRM 
 Scenarios
Customers
Customer 
 Sales Contact Cross References
Leads
Opportunities
Prospects
Prospect 
 Sales Contact Cross References
Territories