How Customer Order Blanket Line/Releases Affect Inventory

When you add a line/release to a blanket line, and the status is set to Ordered, the system increases the Alloc Order (allocated to order) field in Inventory. If you changed the status to Planned, the system does not change the Alloc Order field.

When you change a line/release status from Planned to Ordered, the system increases the Alloc Order quantity in Inventory by the quantity of the line/release. At the same time, the system updates the line/release Ready Quantity (which shows up in Order Shipping) from zero to the amount that is actually ready, if the Reference type is Inventory.

When you ship a line/release, the system decreases the Alloc Order quantity for the item by the Qty Shipped.

NOTES:

Customer Balances

When you add a line/release with a Planned status, the system does not perform any customer credit checks or update customer balances. However, when you change the line/release status from Planned to Ordered, the system performs a credit check, and updates the customer balance to reflect the domestic currency on the line/release being changed. As a result, the system does not increase customer balances for future shipments.


Related Topics

Customer Orders Overview

Creating a Blanket Order