Customer Orders Overview
A company creates and uses a customer order (often 
 abbreviated CO) when it sells goods or services. Each time a customer 
 requests goods or services, a new customer order must be created or changes 
 made to an existing one in the system.
The customer order consists of two major parts: the 
 header and the associated lines/releases. The header, defined 
 on the Customer 
 Orders form, contains information about the customer to whom the 
 items are being sold (such as billing and shipping addresses) and other 
 general information about the order (such as tax information, the total 
 weight, and total price).
The header also contains a field that indicates the 
 type of order: Regular or Blanket. A blanket customer order 
 differs from a regular customer order in that it allows for multiple release 
 dates for each ordered item.
Each customer order (regular or blanket) can have 
 associated multiple line/releases, which you define on the Customer Order 
 Lines or Customer 
 Order Blanket Lines forms. Usually, a line/release is needed for 
 each item being sold. The line/release contains information such as the 
 item number from the Items 
 form, the quantity being sold, and the unit price.
Features
Listed below are some of the features of the Customer 
 module:
	- Maintains detailed customer information
- Supports centralized and decentralized order entry
- Maintains multiple ship-to addresses per customer
- Allows separated drop-ship addresses per line/release
- Allows multiple line/releases per order
- Allows blanket line/releases per order
- Monitors customer order statuses, at multiple levels
- Ties customer orders to multiple manufacturing jobs and purchase 
	 orders
- Allows multiple deliveries and order releases
- Allows customers and customer orders to be placed on credit hold
- Prepares invoices and credit memos
- Has the capability to post to the Financial system
- Determines domestic currency value of outstanding orders
- Reports past-due orders
- Reports gross margin
- Maintains a complete order history system
- Allows orders to be copied from estimates
- Allows easy creation of jobs and POs for line/releases
- Provides numerous sales reports
- Allows quick creation of customer orders through the Customer Orders 
	 Quick Entry form.
Interfacing with Other system Modules
The Customer module interfaces with other system modules 
 as follows:
	- Vendor/Purchasing - Customer 
	 order line/releases can be satisfied by POs. POs can be created automatically 
	 from customer orders using the cross-reference feature.
- Material/Inventory - Line/release 
	 prices and quantity availability information are based on the Items 
	 record. The Items fields, Alloc Order and Sold YTD, 
	 are incremented by the addition and invoicing of customer orders. 
	 The Items record's On Hand quantity is increased or 
	 decreased by customer order returns and shipments.
- Production/Jobs - Customer order 
	 line/releases can be satisfied by jobs. It is possible to create job 
	 orders automatically from customer orders using the cross-reference 
	 feature.
- Estimating - Estimate orders 
	 can be copied to customer orders.
- MRP and APS - Customer orders 
	 appear as outstanding requirements.
- Financial/Accounts Payable - 
	 Salesperson commission information can be accessed during AP Check-Generation 
	 (payment of outside salespersons).
- Financial/Accounts Receivable 
	 - The customer's credit limit is analyzed each time an order is entered 
	 and the system warns you when the customer has exceeded the credit 
	 limit. The invoices and credit memos are generated and printed through 
	 Order Entry and posted to the Accounts Receivable Invoice, 
	 Debit and Credit Memo Transaction form.
- Payroll - Inside salesperson 
	 commissions can be included in the Payroll Transaction Generation 
	 feature.
- General Ledger - All material 
	 transactions associated with customer order shipments and returns 
	 generate entries in the CO Distribution Journal.
- Product Configuration - The addition 
	 of a planning item to a customer order line/release allows an item 
	 to be configured based upon the planning item options. If this is 
	 an item which has not been previously added on the Items form, 
	 it can be created at that point.
- Data Collection - Shipping transaction 
	 information gathered by a data collection solution is used to update 
	 the shipped fields of the appropriate customer order line/releases.
Where Does the CO Number Appear?
The CO number is referenced in the following places:
	- On a PO line/release cross-reference
- On a Job Material cross-reference
- On the Job header
Related Topics
Changing 
 Order Status to History
Configuring 
 a Customer Order
Configuring 
 an Item from a Customer Order Line (Regular or Blanket)
Creating a Customer
Deleting 
 a Customer Order
Invoicing 
 a Customer Order
Order Entry Steps
Setting 
 Up Customer Order Entry
Shipping 
 Customer Orders
About Credit Hold
Change 
 CO Line/Release Status Utility
Change 
 CO Status Utility
Copy Orders 
 And Estimates
Customer 
 Order Blanket Lines
Customers
Delete Customer 
 Orders
About 
 Customer Order Entry for Non-Inventory Items