The system prepares the outbound data for the translator and eventual export to your vendors and customers. Outbound processes include the following:
Posting or printing an appropriate transaction in SyteLine initiates the outbound data flow. This action drives data into the EDI database tables.
The interface then extracts transactions from the EDI database tables and formats them into flat ASCII files that the translator will process.
You may send a customer purchase order acknowledgments. As the interface is processing an incoming purchase order, the system checks to see if the customer is to be sent purchase order acknowledgments. The purchase order acknowledgments are created in the database at the time the purchase orders are posted from EDI to SyteLine or by running the standard system Order Verification Report after the purchase order becomes a customer order in SyteLine.
The Infor SyteLine EDI interface supports the following outbound transactions to your customers.
The Infor SyteLine EDI interface supports the following outbound transactions to your vendors.
Infor SyteLine EDI creates a transaction record for outbound files.
Data from the EDI database tables is formatted into a flat ASCII file. This formatted file is exported to the translator. The files are named as listed below, where the XXX suffix for datafiles corresponds to the Trading Partner code from the EDI Parameters form (both Supply and Demand), and the HHMM.JJJ indicates the time and Julian date for the archive file.
| Trans Type | Data Dir Filename | Archive Dir Filename |
|---|---|---|
| 810 (Header) | IINV_HDR.XXX | INVH(HHMM.JJJ) |
| 810 (Detail) | IINV_DTL.XXX | INVD(HHMM.JJJ) |
| 830 | 830_WRK.XXX | 830(HHMM.JJJ) |
| 850 | 850_WRK.XXX | 850(HHMM.JJJ) |
| 855 | 855_IMP.XXX | ACK(HHMM.JJJ) |
| 856 (Header) | SSEQ_HDR.XXX | SEQH(HHMM.JJJ) |
| 856 (Detail) | SSEQ_DTL.XXX | SEQD(HHMM.JJJ) |
| 862 | 862_WRK.XXX | 862(HHMM.JJJ) |
If necessary, Infor SyteLine EDI can resend the outbound file. You can determine the range of information to be included in the files, and the program sets thePosted flag to No, at which time you can resend the outbound transactions.
Infor SyteLine EDI creates reports on the outbound transactions according to the ranges that you specify.
Infor SyteLine EDI's purge utilities allow you to purge outbound files according to selected ranges. You can delete posted transactions only.
Electronic Data Interchange (EDI) Overview