Pack Confirmation Scenarios
On the Pack Confirmation form, you determine what quantity of
the total picked to put into each package.
- If one item line is selected, and that item is not serial tracked:
- If one line is selected and the item is serial tracked:
- If quantity = 0 then quantity = number of checked serial numbers
- If the number of packages = 0, then the number of packages
= picked quantity of checked serial numbers / quantity.
- The logic works the same as the above examples and only check
serial numbers are moved to packages.
- If a valid package number is entered, the picked quantity is put
into that existing package. If the picked quantity is to be split
between multiple packages, the first part of the picked quantity is
placed into the exiting package and the rest is put into new packages.
Related Topics
Creating
Packages
Picking,
Packing, and Shipping Overview