Creating Packages
To create packages:
- On the Pack Confirmation
form, select a shipment.
- Select the item or items to add to the package.
- Specify the Weight, Rate Code, NMFC
Code, and Marks and Exceptions.
- Select the Hazardous check box if necessary.
- Specify the Package Type
and Package Description.
- Click Create/Add to Package.
A package is created and displayed in the lower left grid. Items and
serial numbers are displayed in the lower right grid.
- When all of the items are in a package, click Process.
Related Topics
Pack
Confirmation Scenarios
Picking,
Packing and Shipping Overview