Creating a Pick List with the Pick Workbench
To use the Pick
Workbench to create a pick list:
- Select a picker.
- Select the lines to include on the pick list. The lines do not
have to have the same due date.
Note: You can
only group together credit card orders (Payment Type C) with other
credit card orders for the same customer and Ship To address.
- Change the group number for each selected line so that they all
have the same group number, which puts them on the same pick list.
- On the Inventory tab, select each line individually. If necessary,
change the Qty To Pick value
in the lower left grid.
- Optionally, you can preassign the serial numbers to be picked,
in the lower right grid.
- If you have more than one pick list in different groups on the
Orders tab, and you want one pick list that includes all of those
pick lists, then select Generate Bulk Pick List. This allows
the picker to pick all the items on more than one pick list with one
trip through the warehouse.
- Click Generate to print the pick
list or lists.
Related Topics
Picking,
Packing and Shipping Overview