A delivery order (DO) consists of three parts:
Create the DO header using the Delivery Orders form. Enter the customer and ship to information to which the lines and sequences will be linked. To add a drop ship to a delivery order, the drop ship information must be manually entered on the Consignee tab after creating the delivery order header.
NOTE: Customer and ship to values are required if you will add sequences during CO shipments. If a generic delivery order is needed, you may leave the Customer and Ship To fields blank. DO lines can be added to a generic delivery order.
Create the DO lines using the Delivery Order Lines form. Each line represents one container/package. It is possible to create the lines at the same time as the sequences (using the Generate Delivery Order Line Sequences form), either by entering a valid line number with each sequence or by leaving the Line field blank and letting the system generate a line number. If an invalid line number is entered, the system displays an error message.
If you have drop ship addresses specified at the order line level, you must create separate delivery orders for each customer order line that has a different drop ship specified. Customer order lines with the same drop ship can be combined into a single delivery order. Entering a delivery order header defaults in the consignee address from the customer specified on the customer order header. There is no functionality to default in the consignee address from a drop ship.
CAUTION: When adding a customer order line that has a drop ship specified that is different than the DO consignee customer information, no warning messages are generated.
If you plan to create the sequences during shipping, either specify a valid line number or leave it blank to allow the system to create a new line number. If you plan to create the sequences after the shipment (using the Generate Delivery Order Line Sequences form), then you can wait until after shipment to create the lines.
Delivery order line sequences can be created during order shipment or after order shipment.
NOTE: To assign many pending shipments at once, select Actions > Mass DO Assignment.
When you process the pending shipments, delivery order line sequences are automatically created for each shipment for which you assigned a DO number.