To receive a purchase order, do the following:
If you are receiving a material that is cross referenced to a job, order, or project, you must have additional permissions in order to complete the receipt. See Receiving Cross-Referenced Items for additional information.
To receive items returned from a customer, use the RMA Return Transaction activity. For more information, see the About Return Receipt help topic.
When you enter a purchase order receiving transaction for a serial number-tracked item, you should be aware of certain special cases. See Handling PO Receipts and Returns for Serial Tracked Items.
Landed cost (freight, duty, etc.) field values will default from the purchase order item during receiving.
When the purchase order is received, landed cost receipt records are created for each of the landed cost amounts on each PO item. The amounts on the landed cost receipt record are in the currency of the landed cost vendor.
You can update the landed cost amounts either in the PO currency by using the fields on the Detail tab, or in the landed cost vendor's currency by using the fields on the Landed Cost tab. If you override a landed cost amount on the Detail tab, it is updated on the Landed Cost tab in the foreign currency, and vice versa.
Any modifications of the landed costs at receiving updates the purchase order line. When a standard cost item is received, the landed costs on the purchase order line are compared to the standard landed costs on the Items form. Any variances are written to the PO Distribution Journal.
A General Ledger transaction is created that debits the Inventory and credits the Accounts Payable, Duties Payable, Freight Payable, Brokerage Payable, Insurance Payable, and Local Freight Payable Accounts, if applicable. When the landed cost amounts are posted to the General Ledger, each of the amounts is converted from the vendor's currency to the domestic currency based on the transaction date's exchange rate.
If Standard costing is used, the following occurs:
If Actual costing is used, the following occurs:
If actual values are unknown at the time of the receipt, the values default from the purchase order line item costs.