Receiving Cross-Referenced Items
Use the Purchase 
 Order Receiving form to receive an item on a purchase order that 
 is cross-referenced to a customer order, a job, or a project.
NOTE: If the purchase 
 order line item you receive is cross-referenced, you may need additional 
 permissions to successfully complete the transaction.
	- On the Purchase Order Receiving form, select a Vendor.
- Update any header information, if necessary, such as GRN Receipt, 
	 Packing Slip, or Trans Date.
- Select a purchase order.
- Update any information about the selected PO.
- Click Receive to receive the PO. The next step in the transaction 
	 varies depending on the type of cross-reference associated with the 
	 item: 
	
		- Order: When a PO line cross-referenced 
		 to a customer order is successfully received, the Order 
		 Shipping form is launched, where you can then ship the 
		 item to the customer who placed the order. 
		At the time of a purchase order receipt, if the item (which 
		 is reserved) is cross-referenced to an order, the system automatically 
		 creates a reservation for the line item equal to the ((qty ordered 
		 - qty shipped) + (qty returned - qty reserved)) up to the amount 
		 that was received. If more is received, the extra goes into inventory. 
- Job: When a PO line cross-referenced 
		 to a job is successfully received, the Job 
		 Material Transactions form is launched to issue the item 
		 directly to the job that it is cross-referenced to. Then go to 
		 the Post 
		 Job WIP Move Transactions form to move the material received 
		 from the PO onto the job.
- Project: When a PO line cross-referenced 
		 to a project is successfully received, the Project 
		 Resource Transactions form is launched.
- SRO: When a PO line cross-referenced 
		 to a SRO is successfully received, the Service 
		 Order Transactions form is launched. 
 
In all cases, a successful PO Receiving transaction 
 is committed whether or not the cross-reference function is successful. 
 If the cross-referenced function is not successful because you lack the 
 required permissions, the receipt transaction is not backed out.
Related Topics