RMA Setup

To tailor RMA to your business, the system offers several codes and parameters that you define to support your processes or to track issues.

The forms you use to set up RMA are:

NOTE: These codes offer you a wide range of options to shape the system for your business. If you make a few key decisions the first time you set up the system, it's easy to make modifications later to achieve more optimum results.

First time. Choosing options on the RMA Parameters form is central to creating a workable RMA system. On the RMA Parameters form, enter answers to the following questions:

  1. Should RMA numbers generated by the system have a prefix?

    We recommend that you enter in the RMA Prefix field a prefix, using R, or RMA, or some other letters you will remember easily. The prefix ensures that your RMAs and your customer orders do not become intermixed. The prefix and separate numbering scheme can be helpful in distinguishing credits from invoices when printing credit memos.

  2. Do you want to charge a fee for handling a customer return?

    If so, enter in the Restocking Fee % field the default percentage to charge.

  3. What do you want to call this fee?

    The system always refers to this fee internally as the "Restocking Fee." However, if you prefer another name, you can enter that name in the Description field. On the RMA credit memo, the fee you charge is then described by the name you prefer.

  4. What location in your warehouse should receive returned materials?

    Enter in the Location field the default location where returned materials are to be received. Typically, this is a non-nettable location (that is, a location for which the Non Nettable Stock field is selected on the Locations form).

  5. What account should be assigned to receive the restocking fee amounts?

    Enter in the Restocking Fee Account field the account number from the General Ledger and any unit codes that apply.

Ongoing. During initial setup, or on an as-needed basis thereafter, you can add and define codes that help you record helpful information about individual entries and track issues across all your returns. The four code forms vary in the level and kind of information they help you track:

Problem, disposition, and evaluation codes can all be tracked using the RMA Status Report. Since these three codes are tracked through a standard report, you should choose codes that describe issues that management wants to track (perhaps to identify future quality goals or achieve current ones).


Related Topics

Return Material Authorization Overview

RMA Steps

About Credit for Returns

About RMA Replacements

About Return Receipt

About Returns

Creating a Rework Order