About Credit for Returns
Determining How Much Credit to Issue
The decision about how much credit to issue is made when the customer
is authorized to reject material on the RMA
Line Items form. Factors that enter into the calculation of the
credit include:
- Quantity to Return. You enter
the number of items for which return is authorized. If the material
is referenced to a customer order and line item, then the quantity
returned cannot be greater than the quantity invoiced. If the item
is serial-tracked, then the quantity returned must be a whole number.
- Unit Credit. You can enter the
credit which you authorize for each unit returned. The default is
the cost associated with the item on the original customer order,
if known, or the cost taken from current pricing routines if the item
is inventoried.
- Restocking Fee. Your company
can elect to charge customers a small fee for the staff time it takes
you to process the returned material. This fee is often called a restocking
fee, but you can call it something else on your credit memos simply
by changing the name in the Description field of the RMA
Parameters form. The system calculates the restocking fee
based on the Restocking Fee % stored on the RMA Parameters
form to provide a Restocking Fee amount. This percent and amount
can be overwritten. Overwriting either one will cause the other to
be recalculated.
NOTE:
- If an RMA line item references a valid customer order and line,
then an attempt is made to back out the commission given on the
original order by the RMA amount. In the calculation of the commission
to reverse, the restocking fee is not included.
- All invoicing (and crediting) must be done at the shipping
site. All accounts receivable and inventory transactions also
occur at this site.
Printing and Posting the Credit
RMA Status Report
First, to preview all RMA line items that are ready to be credited,
run the RMA
Status Report. RMA line items appear on the RMA Status Report
when:
- The Return check box is selected and the quantity returned
is greater than the quantity credited thus far, OR the Return
check box is cleared and an amount remains to be credited.
- RMA line items have a status of Open or Filled. (RMA
line items with a status of Closed or History cannot
be printed or posted.)
- The RMA associated with the RMA line item has a status of Open.
(Items associated with headers which have a status of Stopped,
Closed, or History cannot be printed or posted.)
After reviewing the records pulled by the report, you might want to
modify the range of RMA numbers or of RMA dates, to eliminate records
that should not be receiving credit memos at this time.
RMA Credit Memo
Second, to print RMA credit memos and to post the credits to Accounts
Receivable, perform the RMA
Credit Memo activity.
Printing. The RMA credit memo is printed
on the same special form as the standard invoice. The words RMA CREDIT
will print beneath the header information to differentiate the two documents.
- Form alignment. You can print a sample credit memo using Xs and
9s to represent data fields.
- Restocking Fee. The restocking fee will print on the RMA credit
memo with the label defined by you on the RMA Parameters form.
If you do not charge your customers a fee to return merchandise, do
not enter any label in the Description field on the RMA
Parameters form. That way, no label prints on the credit memo.
- Multi-lingual credits. If the customer is flagged for multi-lingual
invoices, the credit memo will automatically be printed using the
same language for labels.
- Non-domestic currency. The amount posted is always credited in
the customer's currency, even if the amount printed on the credit
memo was translated to the domestic currency.
- Preprinted forms. Be sure to specify whether you use new Moore
forms (the default) or the previously available (old) Moore forms.
- Pre-numbered forms. If your company uses preprinted
and pre-numbered forms, the maximum number of lines allowed per
credit memo is defined on the Accounts
Receivable Parameters form. The invoice headers are the same
but the credit memo number changes. Also, the total amount prints
in words on the footer.
Posting. As part of the posting process,
the status of all RMA line items that have been fully credited is automatically
changed to Closed. If all RMA line items associated with an RMA
header have a status of Closed, then the RMA header status is also
changed to Closed.
- Accounts. The account numbers which will be debited and credited
when you post credits are pulled as follows:
- If the item exists in the Items
form, from the End User Type (if specified) or the Distribution
Account record
- If the item does not exist in the Items form,
from the End User Type (if specified) or Accounts Receivable
Parameters (sales discount account and unit codes).
Adjustments Calculated by the System
Associated adjustments. When customers
reject material for which they received a discount, or for which a sales
representative received commission, then the system adjusts those calculations
where possible.
Both the order level and line item level sales discounts (if
any) given on the original customer order will be backed out if:
- The original customer order and line are known.
- The item on all RMA line items matches the item on the associated
customer order line items.
NOTE: The amount
of sales discount to back out is adjusted to reflect any differences in
the unit price on the original order and the unit credit on the RMA line.
The amount on which the sales commission is figured is adjusted by the
amount of the credit (prior to the application of the restocking fee)
if:
- The RMA line item references a valid customer order (including
History orders) and line.
- The RMA line item exists in the Items form and is the same
as the item on the original customer order.
- There were commissions associated with that particular item on
the original customer order.
Accounts Receivable. When you print
an RMA credit memo, the document is assigned a number which prints in
the Invoice No space. However, the RMA credit appears in Accounts
Receivable as an open credit, with an invoice number of 0.
Related Topics
Return
Material Authorization Overview
Issuing
a Credit
RMA Steps
About
RMA Replacements
About
Return Receipt
About
Returns
RMA Setup