Sending a Communication to a Group of Contacts
You can use the Communication Wizard 
 to send a communication to a group of contacts. This topic includes this 
 information:
For additional information about MailMerge and SyteLine, 
 see Inserting MailMerge Fields 
 for SyteLine 
 Contacts. That topic applies both to communications that use a template 
 and those that do not use a template.
Preliminary Steps
Start with these steps for any type of communication:
	- Decide on the type of communication you plan to send: News, Promotion, 
	 or Other Communication.
 
	- Decide on the method of communication you plan to send: Fax, E-mail, 
	 or Letter. (If you plan to communicate with Portal users, only e-mail 
	 is available, and the rest of these preliminary steps do not apply; 
	 see Sending an E-mail 
	 to Portal Users.)
 
	- Use the Contact Groups form 
	 to create a group of contacts for this communication, if no existing 
	 group meets your needs.
 
	- Ensure that the contacts to whom you want to send the communication 
	 are signed up to accept that type and method of communication from 
	 you. Go to the Sales Contacts 
	 form, Preferences tab, and verify the settings for each contact.
 
	- Open the Communication Wizard 
	 form and continue with the appropriate steps: 
	
 
Sending an E-mail to 
 Portal Users
	- Determine the type of communication you plan to send: News, Promotion, 
	 or Other Communication.
 
	- In the Communication Wizard, 
	 select Portal Users. The Communication 
	 Method defaults to E-mail. 
	 The list of portal users who will receive the communication is based 
	 on those who have subscribed to the publication SpecialPromotionsAnnouncements 
	 through their portal profile.
 
	- Type your message in the Message body. Templates and MailMerge 
	 fields are not available for use with Portal communications.
 
	- Specify the Subject.
 
	- Click Next.
 
	- Select an Interaction Topic and, optionally, specify a note about 
	 the interaction. The Type defaults to E-mail.
 
	- Click Finish. The system 
	 sends the e-mail to portal users through the Application Event System.
 
Sending 
 a Fax or Letter to a Group of Contacts
	- Follow the Preliminary Steps.
 
	- If you are using a template, ensure that you have created a Word 
	 template appropriate for this communication, with MailMerge fields 
	 embedded. See Inserting MailMerge 
	 Fields for SyteLine 
	 Contacts.
 
	- In the Communication Wizard, 
	 specify the Communication Type.
 
	- Specify the Communication Method as Fax 
	 or Letter.
 
	- Select the group you defined in the Preliminary 
	 Steps.
 
	- Click Next. The contacts 
	 from the group who have specified that they want to receive this type 
	 and method of communication are listed.
 
	- Select the contacts that you want to include in this communication.
 
	- Click Browse and select 
	 the template you defined in step 2.
 
	- The system responds by creating a .csv file that contains one record 
	 for each contact, with the available MailMerge field values for that 
	 contact. You are prompted to open the file. If you want to verify 
	 the values, click Yes. Close 
	 the file when you are finished.
 
	- The text from the template, including the MailMerge fields, is 
	 displayed in the Message field. You cannot edit the text.
 
	- Click Next. A Microsoft 
	 Word file is created that includes one copy of the merged document 
	 for each contact. 
 
	- Print the document.
 
	- Click Finish to close the 
	 Communication Wizard.
 
	- Fax or mail the printed documents to the individual contacts.
 
Sending 
 an E-mail “Blast” to a Group of Contacts
You can use the SyteLine 
 MailMerge fields either in a template or in a simple text message.
Using a MailMerge Template with HTML Formatting
If you specify a Microsoft Word template (using either of the file extensions 
 .docx or .dotx) and use MailMerge, your e-mail is sent through your installation 
 of Microsoft Outlook. The e-mail is created as an HTML document with merge 
 fields embedded in it. Use these steps:
	- If you want to send these e-mail blasts from a special “Marketing” 
	 e-mail address rather than from your personal address, add the Marketing 
	 e-mail account to your Outlook Profile and temporarily set that profile 
	 as the default.
 
	- Ensure that you have created a Word template appropriate for this 
	 communication, with MailMerge fields embedded. See Inserting 
	 MailMerge Fields for SyteLine 
	 Contacts.
 
	- Follow the Preliminary Steps.
 
	- In the Communication Wizard, 
	 specify the Communication Type.
 
	- Specify the Communication Method as E-Mail.
 
	- Select the group you defined in the Preliminary 
	 Steps.
 
	- Click Next. The contacts 
	 from the group who have specified that they want to receive this type 
	 and method of communication are listed.
 
	- Select the contacts from the group to be included in this communication 
	 and click Next.
 
	- Click Browse and select 
	 the template you defined in step 2.
 
	- The system responds by creating a .csv file that contains one record 
	 for each contact, with the available MailMerge field values for that 
	 contact. You are prompted to open the file. If you want to verify 
	 the values, click Yes. Close 
	 the file when you are finished.
 
	- The text from the template, including the MailMerge fields, is 
	 displayed in the Message field. Do not edit the Message text in the 
	 form.
 
	- Specify a Subject for the communication.
 
	- Click Next.
 
	- The E-mail Blast populates the Word template with data from your 
	 selected contacts and e-mails each record separately from your Outlook 
	 profile. Sent e-mails can be viewed in your Outlook Sent Mail folder
 
	- In the Communication Wizard, 
	 log information about the communication. See the field descriptions 
	 for more information: 
	
 
	- Click Finish to save the 
	 log information.
 
Sending a Blast E-mail without a Template
You can also send an e-mail that is either basic text formatting or 
 HTML, typed directly into the Communication 
 Wizard form, and not using 
 a template. Blast e-mails that do not use a template are sent out through 
 the application event system.
To set up this type of e-mail:
	- If you want to type HTML formatted text into the Communication 
	 Wizard form, ensure that these event handlers are updated to allow 
	 HTML: 
	
		- In the Event Handlers 
		 form, select GenericSendEmail. 
		 Click Event Actions. Click 
		 Edit Parameters. Ensure 
		 that Body is in HTML Format 
		 is selected and click OK.
 
		- Return to Event Handlers 
		 and repeat the above step for the GenericNotify 
		 and InteractionEmail events.
 
	
 
	- Follow the Preliminary Steps.
 
	- In the Communication Wizard, 
	 specify the Communication Type.
 
	- Specify the Communication Method as E-Mail.
 
	- Select the group you defined in the Preliminary 
	 Steps. 
 
	- Click Next. The contacts 
	 from the group who have specified that they want to receive this type 
	 and method of communication are listed.
 
	- Select the contacts from the group to be included in this communication 
	 and click Next.
 
	- Type a Subject and enter your text in the Message field. You can 
	 include SyteLine 
	 MailMerge fields (see Inserting 
	 MailMerge Fields for SyteLine 
	 Contacts). If HTML is allowed (see step 1), you can type in basic 
	 HTML formatting such as <b>text</b> 
	 in your message text.
 
	- Click Next.
 
	- In the Communication Wizard, 
	 log information about the communication. See the field descriptions 
	 for more information: 
	
 
	- Click Finish to save the 
	 information.
 
Related Topics
Inserting 
 MailMerge Fields for SyteLine Contacts