Communication Wizard
	
	This form allows you to send various types of communications to 
	 a sales group or to individual members of a sales group. Sales communications 
	 can be saved and viewed on the Sales Contacts form.
	You can also send promotional e-mails to Customer Portal users from 
	 this form. If you select this option, certain fields are disabled 
	 and some steps in the wizard are skipped.
	For sales contact communications, the wizard has four steps:
	
		- Identify Communication Type and 
		 Method: This step defines the type of communication and the 
		 group of contacts (or portal users) with whom you will be communicating.
 
		- View and Select Sales Contacts: 
		 In this step, you choose which contacts in the group you will 
		 include in the communication. Contacts only display in this step 
		 if their interaction 
		 permissions allow the selected method of communication.
 
		- Identify/Create Template: 
		 This step is where you define the content of the message. If you 
		 are using a Microsoft Word template, select it here. If you are 
		 sending an e-mail communication, you can use MailMerge fields 
		 to personalize the message. This is the point at which the message 
		 is either printed out (for fax or mailing) or e-mailed (via Outlook 
		 or the Application Event System).
 
		- Log Communication: In this 
		 optional step, you log information about this interaction. Log 
		 entries are viewable on the Sales 
		 Contacts, Campaigns, 
		 Customers, and Prospects 
		 forms, depending on the group you selected during the Identify 
		 Communication Type and Method step.
 
	
	For more details about how to use the Communication Wizard, see 
	 these topics: 
	
	
Related Topics
CRM Overview
Sending a Communication to a Group of Contacts
Inserting MailMerge Fields for SyteLine Contacts
Prospects
Sales Contact Groups
Sales Contacts