Using RMA Extended Dispositions
These steps illustrate an example process that you can for an RMA item
that requires extended disposition.
Create an RMA
To create a Return Material Authorization (RMA):
- In the RMAs form, create
a new RMA record.
- Specify a customer.
- Specify the warehouse. It must match the Disposition Warehouse
specified in the RMA Parameters
form.
- Save the record.
- Click RMA Lines to open
a linked RMA Line Items form.
Create an RMA Line
To create a Return Material Authorization (RMA) line:
- In the RMA Line Items form,
specify an item and the quantity to be returned.
- On the Dispositions tab, verify that the Use
Disposition Process field is selected. (This value is defaulted
from the RMA Parameters form.)
- Save the record.
Create a Disposition Entry for the RMA Line
To create a disposition entry for each RMA line:
- In the RMA Item Dispositions
form, create a new disposition record.
- Specify your RMA and line for disposition. In the lines section,
values for the Item, quantity to return, Use Disposition Process,
and disposition code are defaulted from the RMA line.
- Specify the disposition code and the quantity to be dispositioned.
Disposition codes are created on the Disposition Codes form.
- If a serial number should be preassigned to the returned item,
click Serial Numbers to open
the modal RMA Item Serials
form. Assign the number and return to the parent form.
- In the Return To Vendor section, specify the vendor of the item.
- Save the record. The Qty Disposition field for the line is updated
to show the quantity to disposition.
Process the RMA Disposition
To process the item returned to you from the customer:
- On the RMA Return Transactions
form, specify your RMA number.
- In the grid, select Selected and clear Return To Stock.
- Click Receive. A message shows the number of transactions
posted.
Post the Disposition
To post the disposition:
- In the RMA Item Dispositions
form, click the Refresh toolbar button to display any changes if you
have the form open. If the form was closed, reopen it and specify
your RMA number.
- Note the changes: The Qty Received field now displays the quantity
received through the RMA return transaction.
- Click Post Disposition. The line status is changed to Filled,
and the Posted check box is selected.
Perform Vendor Shipping
To perform the vendor shipping transaction:
- In the Vendor Shipping
form, specify the vendor from the RMA
Item Dispositions form.
- Select the grid line with RMA in the Reference field and your RMA
number in the Ref Num field.
- Click Ship Line. A message informs you that the vendor shipment
will be performed.
- Click OK. After shipping
is performed, your line is removed from the grid.
Perform Vendor Return
To perform the vendor return transaction:
- In the Vendor Returns form,
specify the vendor from the RMA Item
Dispositions form.
- Select the grid line with RMA in the Reference field and your RMA
number in the Ref Num field.
- Click Return Line. A message
informs you that the vendor return will be performed.
- Click OK. After return
shipping is performed, your line is removed from the grid.
Verify Disposition
To verify the disposition updates:
- In the RMA Item Dispositions
form, click the Refresh toolbar button to display any changes if you
have the form open. If the form was closed, reopen it and specify
your RMA number.
- Verify that the Qty Moved field displays the quantity that was
shipped or received.
Related Topics
About
RMA Extended Dispositions
RMA
Extended Disposition - Accounting Information
Setting
Up RMA Extended Dispositions
About
Returns