Use the A/P Check Printing/Posting form to:
Checks that you post from A/P contain the reference type A/P and a reference number corresponding to the vendor number of the A/P check. During posting, multi-currency gains and losses are recorded to the A/P ledger distribution journal (if applicable).
NOTE: If a discount is taken, the Discount field prints by itself on the line immediately following its corresponding voucher information. This line will also print the side label Discount whenever the line prints.
When you print and post checks, three vendor fields are updated:
It is possible to modify the system so that you can print checks in a language other than your domestic language. To do so, you must modify the Source Code for the two stored procedures that handle A/P Check Translation: WordNumSp() and WordNumISp(), which are included with all SyteLine distributions.
Check amounts print as both words and numeric amounts. Two lines are available to display the amount in words. Check amounts are limited to print billions or less. If the currency code is MXN or MXV, the check amount prints in Spanish, regardless of the specified language code, and billions are represented as "thousands of millions."
You can also use the A/P Check Printing/Posting form to void checks.
NOTE: If you exit from this form after printing or voiding checks but without running the Final Register and Post option, the system will void any records that are not already voided, and then automatically run the Final Register And Post option.
After you print or void standard checks, you have the option to print copies of the check stubs.
If the Manual option for Remittance Advice is selected on the Accounts Payable Parameters form, you must also select Print Remittance Advice.
TIP: To have the remittance advice statement processed for print, fax, or e-mail on a vendor-by-vendor basis, also select the Use Profile check box.
NOTE: If you select this option but no manual checks exist in the check batch, the remittance advice will be blank.