Voucher Adjustment Distribution

Use the Voucher Adjustment Distribution form to specify how to distribute transactions to multiple G/L accounts.

You can distribute to the G/L accounts, using two methods:

Use the tax fields to record the detailed tax records that are associated with the voucher and appear on the tax reports. Each tax system-tax code-exempt tax code combination should contain one tax distribution record.

The fields on the header and General tab are display only. Their values are extracted from the A/P Vouchers and Adjustments form.

You can make several types of distributions, such as purchase amount, freight, and tax. The system sets the fields when you post them from a PO or from the Generate Distribution option for directly entered vouchers.

Because vouchers may contain a mixture of taxable and non-taxable amounts, you may overwrite the standard tax calculation. To do so, update the Amount fields of tax-related G/L Distribution records. These changes are reflected in the tax fields of the voucher header (which you cannot update directly).

This feature enables you to manually enter tax-only debit and credit memos, as well as the tax for mixed invoices.

NOTES:


Related Topics

Accounts Payable Steps

Distributing Vouchers and Adjustments