Distributing Vouchers and Adjustments
You can manually or automatically create distributions
for vouchers and adjustments. You can also have the system distribute
the amounts for you during the posting process.
Manually Distributing Vouchers and Adjustments
To distribute vouchers and adjustments manually:
- Open the Voucher
Adjustment Distribution form.
- To add a distribution, select Actions > New.
- In the Vendor field, select the vendor whose voucher or
adjustment you want to distribute.
- In the Voucher field, select the transaction you want to
distribute.
- In the Dist Seq field, accept the default value of the next
available sequence number.
This number is used to order the distributions for the selected
transaction.
- On the Allocation And Tax tab, in the Amount field,
enter the distribution amount.
- In the Account field, select the General Ledger account
to post the transaction to.
- If you must submit DIOT and IETU reports, specify or review this
information on the Tax Parameters
tab:
Tax Reg Number Type
Specify the tax regulation number.
DIOT Transaction Type
Specify the DIOT transaction type.
Tax Reg Num Foreign
If selected, indicates that the vendor has a foreign tax regulation
number.
Deduction Percent
Specify the percentage deducted from the voucher distribution.
Vendor Name
The vendor name is displayed.
Tax Reg Num
The tax regulation number is displayed.
ISO Country Code
Select the ISO-defined country name.
These fields are only displayed for users who are assigned a Mexico
Localization license.
- Select Actions > Save.
- Repeat steps 1-7 to continue distributing the transaction until
the value in the Distribution Total field on the Amounts
tab equals that of the Invoice Amt field.
Automatically Distributing Invoices and Adjustments
To distribute invoices and adjustments automatically:
- Open the A/P
Vouchers and Adjustments form or the Voucher
Adjustment Distribution form.
- Verify that you are working with the transaction you want to distribute.
- Select Actions > Distribution Generation.
- When prompted, to have the system generate the distributions for
the displayed transaction, select OK.
Related Topics
Accounts Payable
Steps
Posting Vouchers
- Detail