This topic describes in detail the posting of inventory transactions to the General Ledger (GL) module. All transactions processed in the Customer, Material, Vendor, and Production modules that affect the value of inventory are posted to the appropriate inventory distribution journal (CO Dist, IC Dist, PO Dist, and SF Dist, respectively) using account numbers that can be found in the Product Codes, Departments, Purchasing Parameters, and Distribution Accounts forms.
Because the costs and account numbers used for the journal posting are quite different if using standard costing or one of the four actual cost flow methods, the transactions generated are explained for both standard and actual. If the system should not automatically generate these transactions, clear the General Parameters form's Post to Journal check box.
The system uses the same GL account numbers when posting to the appropriate inventory distribution journal, no matter which of the four actual cost flow methods is in use (Average, LIFO, FIFO, Specific). For this reason, the transactions outlined below are for actual costing in general.
The phrase issue cost is used several times in this topic to refer to the cost at which an item is being issued from inventory. The issue cost value varies depending on the cost flow method in use.
Before processing any transactions in the manufacturing modules, the GL account numbers which are used for posting to the GL inventory distribution journals must be set up. The key accounts are stored at the Product Code level, so that different account numbers may be assigned to different classifications of items and also allow for the tracking of cost details of a unit cost.
Maintaining individual accounts for the various cost details allows visibility of these costs through work in process, inventory and cost of goods sold and more accurately determines the exposure relating to material, labor, fixed overhead, variable overhead and outside service costs. It is also possible to use one account number for all the cost detail components of an item if this cost detail visibility is not desired.
A finished goods inventory account number and a raw materials inventory account number may be used rather than having all items posted to the same inventory account.
| Finished Goods Account | Account Number |
|---|---|
| FG INV Material Cost | 1001 |
| FG INV Labor Cost | 1002 |
| FG INV Fixed Overhead Cost | 1003 |
| FG INV Variable Overhead Cost | 1004 |
| FG INV Outside Service Cost | 1005 |
| Raw Materials Account | Account Number |
|---|---|
| RM INV Material Cost | 2001 |
| RM INV Labor Cost | 2002 |
| RM INV Fixed Overhead Cost | 2003 |
| RM INV Variable Overhead Cost | 2004 |
| RM INV Outside Service Cost | 2005 |
These accounts may be used rather than having all items posted to the same inventory account.
| Finished Goods Inventory Account | Account Number |
|---|---|
| FG INV Material Cost | 1001 |
| Labor Fixed Overhead Cost | 1001 |
| Variable FG INV Outside Service Cost | 1001 |
| Raw Materials Inventory Account | Account Number |
|---|---|
| RM INV Material Cost | 2001 |
| Labor Cost | 2001 |
| Fixed Overhead Cost | 2001 |
| Variable RM INV Outside Service Cost | 2001 |
The following lists identify the accounts found in the Product Codes, Departments, Purchasing Parameters, Work Centers, and Distribution Accounts forms.
Inventory Adjustment
Material Fixed Overhead Applied
Material Variable Overhead Applied
NOTE: The Material Fixed Overhead Applied and the Material Variable Overhead Applied accounts are required only when basing overhead on job material issues.
Vouchers Payable Account
Direct Labor Applied Account
Fixed Overhead Applied Account
Variable Overhead Applied Account
Although these rates default from this location, they are also maintainable on the Current Operations, Job Operations, and Estimate Operations forms.
Fixed Machine Overhead Applied Account
Variable Machine Overhead Applied Account
Although these rates default from this location, they are also maintainable at the Current Operations, Job Operations, and Estimate Operation forms.
Inventory Material
Inventory Labor
Inventory Fixed Overhead
Inventory Variable Overhead
Inventory Outside
COGS Material
COGS Labor
COGS Fixed Overhead
COGS Variable Overhead
COGS Outside
In-Transit Material
In-Transit Labor
In-Transit Fixed Overhead
In-Transit Variable Overhead
In-Transit Outside
NOTE: You can delete any distribution account record, including the default distribution account, with a blank warehouse and blank product code.
The inventory account numbers used for journal transactions do not come directly from the Product Codes form. Rather, the inventory accounts used come from the stock location being accessed when the transaction is performed. (When a stock location is added for an item in the Inventory module, inventory accounts are entered for the location, using the Item Stockroom Location form.) The default for this field is the inventory account numbers in the Distribution Account file to which the item belongs.
To locate the inventory account numbers:
If any of the account numbers the system is attempting to use have not been set up, the system does not post to the GL inventory distribution journals.
The following subsections outline every transaction that is posted to the inventory distribution journals when some method of actual costing is being used.
The following transactions are posted to the inventory distribution journal named PO Dist.
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Vouchers Payable | xxxx |
Because this item is purchased, only one posting (Inventory Material Cost) is applicable. All accounts for each cost details component would have the same account number, therefore only one posting entry is made.
The cost used is the quantity received multiplied by the purchase order line item unit cost. (This is the default cost. At the time of receipt, it is possible for you to update the receipt cost to anything.)
CU = (RQ * POUC)
where:
CU = Cost Used
RQ = Receipt Quantity
POUC = PO Unit Cost
| Transaction | Debit | Credit |
|---|---|---|
| Vouchers Payable | xxxx | |
| Inventory | xxxx | |
| Inventory Adjustment | xxxx or | xxxx |
The cost used is the quantity returned multiplied by the item's issue cost:
CU = (QR * IIC)
where:
CU = Cost Used
QR = Quantity Returned
IIC = Item's Issue Cost
Transaction
a. If vouchered cost > receipt cost:
Vouchers Payable
Accounts Payable
b. If vouchered cost < receipt cost:
Vouchers Payable
Inventory Adjustment
Accounts Payable
The previous transaction is created only if any line items were vouchered at a different cost than the cost at which they were received into inventory. (The cost at which the items were received into inventory is the line item unit cost field at the time of the receipt.)
xxxx = (quantity received * (vouchered cost - receipt cost))
xxxx = (cost of receipt - cost of voucher) - adjustment
POVC = QR * (VC - RC)
where:
POVC = Purchase Order Variance Cost
QR = Quantity Received
VC = Voucher Cost
RC = Receipt Cost
The following transactions are posted to the inventory distribution journal named SF Dist.
| Transaction | Debit | Credit |
|---|---|---|
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Fixed Material Overhead Applied | xxxx | |
| Variable Material Overhead Applied | xxxx |
The inventory accounts used are those of the item being issued to the job, not the item being manufactured. The inventory credit amount is the quantity issued from inventory multiplied by the issue cost of the item.
ICA = QIFI * IC
where:
ICA = Inventory Credit Amount
QIFI = Quantity Issued from Inventory
IC = Issue Cost
The credits to the overhead accounts are calculated by multiplying the actual material cost by the fixed and variable overhead rates in the Product Codes form.
COA = MC * (FO + VOR)
where:
COA = Credits to the Overhead Account
MC = Material Cost
FO = Fixed Overhead
VOR = Variable Overhead Rate
The debit to WIP is the sum of the direct material, fixed overhead, and variable overhead amounts.
DTWIP = DM + FO + VOA
where:
DTWIP = Debit to WIP
DM = Direct Material
FO = Fixed Overhead
VOA = Variable Overhead Amounts
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx | |
| Fixed Material Overhead Applied | xxxx | |
| Variable Material Overhead Applied | xxxx |
The debit to inventory is the quantity of the item withdrawn from the job multiplied by a unit cost figure which varies depending on the costing method in use.
DTI = QIWJ * VUCF
where:
DTI = Debit to Inventory
QIWJ = Quantity of the Item Withdrawn from the Job
UCF = Unit Cost Figure
The debits to the overhead accounts are calculated by multiplying the average cost of all items issued. The job material total actual cost/job material quantity issued.
DOA = MT / JI
where:
DOA = Debits to the Overhead Account
MT = Job Material Total actual cost
JI = Job material quantity issued
The credit to WIP is the sum of direct material, fixed overhead, and variable overhead amounts.
CTWIP = DM + FO + VOA
where:
CTWIP = Credit to WIP
DM = Direct Material
FO = Fixed Overhead
VOA = Variable Overhead Amounts
| Transaction | Debit | Credit |
|---|---|---|
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| Direct Labor Applied | xxxx | |
| Fixed Labor Overhead Applied | xxxx | |
| Variable Labor Overhead Applied | xxxx |
The credit to labor is the actual hours in the transaction multiplied by the specified manufacturing rate of the employee who reported the transaction.
CTL = AH * SMR
where:
CTL = Credit To Labor
AH = Actual Hours
SMR = Specified Manufacturing Rate
The credits to the overhead accounts are calculated by multiplying the actual labor hours by the fixed and variable overhead rates in the Departments form.
COA = LH * (FO + VOR)
where:
COA = Credits to the Overhead Account
LH = Labor Hours
FO = Fixed Overhead
VOR = Variable Overhead Rate
The debit amount to WIP is the sum of direct labor, fixed overhead, and variable overhead amounts.
Machine costs apply machine overhead charges to a job operation for the hours a machine was run, along with the quantity of goods completed, scrapped, and moved to the next operation. If the work center for the operation is machine scheduled, the remaining scheduling time for the operation will be reduced by the total hours posted.
The additional posting described below for the "Move" transaction is also performed for all "Run" transactions.
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx |
When inventory is received from a job, the receipt cost used is determined by:
If the receipt is being performed using a labor transaction on the last operation, you have the option of closing the job order. If the job is closed when the transaction is entered, the receipt cost used is always the actual unit cost of the job. If the job is not closed and the Costs Based on Complete parameter is set to Jobs, the receipt cost used is the planned unit cost of the job.
The planned unit cost is based on the setup, run-times, run rates, and labor overhead rates in the Job Operations form as well as the unit costs and the material overhead rates in the Job Materials form.
If the job is not closed and the Costs Based on Complete parameter is set to Operations, the receipt cost used is determined by the Complete flag of the job's operations. Actual costs from complete operations are accumulated while planned costs from incomplete operations are accumulated to determine the final receipt cost.
| Transaction | Debit | Credit |
|---|---|---|
| a. If actual cost > planned cost: | ||
| Inventory Adjustment | xxxx | |
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx | |
| b. If actual cost < planned cost: | ||
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx | |
| Inventory Adjustment | xxxx |
If the job is being closed manually by changing the status from Released to Complete an adjustment needs to be made since the job's planned cost would have been used for the transaction that put the item to stock.
The amount used is the difference between the total planned and actual cost of the job:
AU = TPC - AC
where:
AU = Amount Used
TPC = Total Planned Cost
AC = Actual Cost
The following transactions are posted to the inventory distribution journal named CO Dist.
| Transaction | Debit | Credit |
|---|---|---|
| COGS Material | xxxx | |
| COGS Labor | xxxx | |
| COGS Fixed Overhead | xxxx | |
| COGS Variable Overhead | xxxx | |
| COGS Outside | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx |
The amount used is the quantity shipped multiplied by the issue cost of the item.
AU = QS * ICI
where:
AU = Amount Used
QS = Quantity Shipped
ICI = Issue Cost of the Item
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| COGS Material | xxxx | |
| COGS Labor | xxxx | |
| COGS Fixed Overhead | xxxx | |
| COGS Variable Overhead | xxxx | |
| COGS Outside | xxxx |
The amount used is the average value of all shipments.
AU = CST / IQS
where:
AU = Amount Used
CST = Item's Cost of Goods Sold Total
IQS = Item's Quantity Shipped
The following transactions (unless otherwise specified) are posted to the inventory distribution journal named IC Dist.
| Transaction | Debit | Credit |
|---|---|---|
| a. Increase quantity: | ||
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Adjustment | xxxx | |
| b. Decrease quantity: | ||
| Inventory Adjustment | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx |
The amount used for an inventory adjustment transaction varies depending on the cost flow method in use. If you are using:
Cycle counting and physical inventory posting create transactions like the ones described above. Either transaction a or b is created, depending on whether the count quantity is greater than or less than the original quantity.
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Adjustment |
This transaction is posted only if the From and To locations have different inventory accounts tied to them or if specific costing is being used and the From and To locations have different unit costs tied to them.
The inventory account debited is the account tied to the To location. The credited inventory account is the account tied to the From location. The inventory adjustment account is used only for specific costing when the From and To accounts have different costs assigned to them.
A transaction is created if you change the inventory account tied to the location:
| Transaction | Debit | Credit |
|---|---|---|
| Inventory (New Accounts): | ||
| Inventory Material Cost | xxxx | |
| Inventory Labor Cost | xxxx | |
| Inventory Fixed Overhead Cost | xxxx | |
| Inventory Variable Overhead Cost | xxxx | |
| Inventory Outside Cost | xxxx | |
| Inventory (Old Accounts): | ||
| Inventory Material Cost | xxxx | |
| Inventory Labor Cost | xxxx | |
| Inventory Fixed Overhead Cost | xxxx | |
| Inventory Variable Overhead Cost | xxxx | |
| Inventory Outside Cost | xxxx |
A transaction is also created if specific costing is in use and you change the unit cost tied to the location.
(This example assumes that all cost detail values are changed.)
| Transaction | Debit | Credit |
|---|---|---|
| a. Increase cost: | ||
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Adjustment | xxxx | |
| b. Decrease cost: | ||
| Inventory Adjustment | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx |
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Adjustment | xxxx |
This transaction is only posted if a quantity is entered for the location at the same time it is added.
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Inventory Adjustment | xxxx |
The debit amount used is the quantity received extended by the unit cost you entered.
DAU = QR * UCEBU
where:
DAU = Debit Amount Used
QR = Quantity Received
UCEBU = Unit Cost Entered by you
The unit cost defaults to the value in the Items form's Unit Cost field at the time the transaction is entered.
The credit account is the GL account number you entered. The account defaults to the item's Inventory Adjustment account.
| Transaction | Debit | Credit |
|---|---|---|
| Account Entered | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx |
The debit account is the GL account number you entered. The account defaults to the item's Inventory Adjustment account.
The credit amount used is the quantity issued multiplied by the issue cost of the item:
CA = QI * IC
where:
CA = Credit Amount
QI = Quantity Issued
IC = Issue Cost
The following transactions are posted to the inventory distribution journal named SF Dist.
| Transaction | Debit | Credit |
|---|---|---|
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx | |
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Fixed Material Overhead Applied | xxxx | |
| Variable Material Overhead Applied | xxxx |
The following transaction(s) are posted to the inventory distribution journal named SF Dist.
| Transaction | Debit | Credit |
|---|---|---|
| Inventory Material | xxxx | |
| Inventory Labor | xxxx | |
| Inventory Fixed Overhead | xxxx | |
| Inventory Variable Overhead | xxxx | |
| Inventory Outside | xxxx | |
| Fixed Material Overhead Applied | xxxx | |
| Variable Material Overhead Applied | xxxx | |
| WIP Material Costs | xxxx | |
| WIP Labor Costs | xxxx | |
| WIP Fixed Overhead Costs | xxxx | |
| WIP Variable Overhead Costs | xxxx | |
| WIP Outside Costs | xxxx |