Posting to General Ledger - Standard Costing

The standard costing system posts all transactions that affect the value of inventory to the GL inventory distribution journals. All transactions are processed using standard costs that have been established with variances being posted to a series of variance account numbers.

General Ledger Account Numbers Used

Before processing any transactions in the manufacturing modules you must set up the GL account numbers to use for posting to the inventory distribution journals. These account numbers can be found in the Product Codes, Departments, Purchasing Parameters, and Distribution Accounts forms.

The following list details the accounts you need to set up.

Product Codes - WIP

WIP Material

WIP Labor

WIP Fixed Overhead

WIP Variable Overhead

WIP Outside

Product Codes - Miscellaneous

Inventory Adjustment

Product Codes - Applied Overhead

Material Fixed Overhead Applied

Material Variable Overhead Applied

NOTE: The Material Fixed Overhead Applied and the Material Variable Overhead Applied accounts are required only when basing overhead on job material issues.

Product Codes - Variance

Purchase Cost

Material Usage

Routing

Product Codes - Labor Variance

Labor Rate

Labor Usage

Product Codes - Overhead Variance

Labor Fixed Overhead Usage

Labor Variable Overhead Usage

Material Fixed Overhead Usage

Material Variable Overhead Usage

Machine Fixed Overhead Usage

Machine Variable Overhead Usage

NOTE: The Material Fixed Overhead Usage and the Material Variable Overhead Usage accounts are required only when basing overhead on job material issues.

Purchasing Parameters

Vouchers Payable

Departments

Direct Labor Applied Account

Fixed Overhead Applied Account

Variable Overhead Applied Account

NOTE: The Fixed Overhead Applied and the Variable Overhead Applied accounts are required only when basing overhead on job labor.

Although these rates default from this location, they are also maintainable at the Current Operations, Job Operations, and Estimate Operations forms.

Work Centers - Costing

Fixed Machine Overhead Applied Account

Variable Machine Overhead Applied Account

Although these rates default from this location, they are also maintainable at the Current Operations, Job Operations, and Estimate Operations forms.

Distribution Accounts - Inventory

Inventory

Inventory Labor

Inventory Fixed Overhead

Inventory Variable Overhead

Inventory Outside

Distribution Accounts - Sales/Cost of Goods Sold

COGS Material

COGS Fixed Overhead

COGS Variable Overhead

COGS Outside

Distribution Accounts - In-Transit

In-Transit Material

In-Transit Labor

In-Transit Fixed Overhead

In-Transit Variable Overhead

In-Transit Outside

NOTE: You are allowed to delete any distribution account record, including the default distribution account with a blank warehouse and blank product code.

The inventory account number used for journal transactions does not come directly from the Distribution Accounts form. Rather, the inventory accounts used comes from the stock location being accessed when the transaction is performed.

When a stock location is added for an item in the Inventory module, an inventory account is entered for the location, and an account number for each cost detail component is added.

The default for these fields are the inventory account numbers in the Distribution Accounts file to which the item belongs.

To locate the inventory account numbers, the system searches, in the following order, for:

The system does not post to the G/L inventory distribution journals if any of the account numbers it is attempting to use are not set up.

Transaction Posting to the Inventory Distribution Journals

Outlined below is every transaction that is posted to the inventory distribution journals when standard costing is being used.

Purchasing Transactions

The following transactions are posted to the inventory distribution journal named PO Dist.

Production Transactions

The following transactions are posted to the inventory distribution journal named SF Dist.

If the quantity of any material issued is more or less than the standard quantity required, the following accounts are adjusted:

The material usage variance amount is the difference between the standard quantity required and the actual quantity issued, extended by the standard cost of the material.

The overhead variance amounts are material usage variance extended by the fixed and variable material overhead rates.

If subsequent to this transaction there is any remaining WIP amount (+ or -), the following adjustment is made.

  Debit Credit
a. If remaining WIP amount is greater than (>) 0 then:    
Routing Variance xxxx  
WIP Material   xxxx
WIP Labor   xxxx
WIP Fixed Overhead   xxxx
WIP Variable Overhead   xxxx
WIP Outside   xxxx
b. If remaining WIP amount is less than (<) 0 then:    
WIP Material   xxxx
WIP Labor xxxx  
WIP Fixed Overhead xxxx  
WIP Variable Overhead xxxx  
WIP Outside xxxx  
Routing Variance   xxxx

This transaction may be necessary since the WIP account is increased with amounts that are based on the standard times and rates that are established for the job. The decrease of the WIP in the job finish transaction is based on the standard cost of the item being manufactured. If the total standards for the job do not match the standard unit cost of the item, this adjustment to WIP needs to be made.

If the job is not closed at the time the job transaction is posted, the above transaction is posted at the time the status of the job is manually changed from (R)eleased to (C)omplete.

Customer Order Transactions

The following transactions are posted to the inventory distribution journal named CO Dist.

Inventory Control Transactions

The following transactions (unless otherwise specified) are posted to the inventory distribution journal named IC Dist.


Related Topics