The NACHA file format is composed of 94-character records.
The File Header and File Control records are the outer "envelope" of the transaction. The Batch Header and Batch Control records act as an inner envelope combining similar entries.
Records can be formatted using the ACH or IAT file structure.
Each record ends with a carriage control (line break) character.
ACH records are used when payments are sent domestically within the United States.
This record includes your company name and company number. It also designates the immediate destination of the entries in the file.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 1. This identifies the file header record. | |
| Priority Code | 2 | 2 | Value is 01. The lower the number, the higher the processing priority. Currently, only 01 is used. | |
| Filler | 4 | 1 | Blank | Not used. |
| Destination ID | 5 | 9 | Fill with zeros to the left | apparms_mst.ach_dest_id - Bank's transit routing number |
| Company ID | 14 | 10 | Left-justified | apparms.ach_co_id - Company number. The use of an IRS federal tax ID number is recommended. |
| Creation Date | 24 | 6 | YYMMDD | dbo.getsitedate - Date the input file was created. |
| Creation Time | 30 | 4 | HHMM | dbo.getsitedate - Time of day the input file was created. |
| File ID | 34 | 1 | Uppercase A-Z Numeric 0-9 | Initial value is A. This is a code to distinguish between multiple input files. If more than one file is delivered, they must have different file IDs. |
| Record Size | 35 | 3 | Value is 094 - Number of bytes per record. | |
| Blocking Factor | 38 | 2 | Value is 10. | |
| Format Code | 40 | 1 | Value is 1. | |
| Destination Name | 41 | 23 | Left-justified | bank_hdr_mst.name - Name of bank. Form field is 60 characters, but is truncated here to 23. |
| Company Name | 64 | 23 | Left-justified | parms_mst.company - Name of your company. Form field is 60 characters, but is truncated here to 23. |
| Filler | 87 | 8 | Blanks | Not used. |
NOTE: There is a space between the File Header Company Name and the Batch Header Record Code.
This record contains the effective entry (transaction) date, which is the date the deposits will be settled. The record also identifies your company and contains an entry description for debits and credits in this batch.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 5. This identifies the batch header record. | |
| Service Class | 2 | 3 | Value is 200. This identifies the type of entries in the batch as ACH Entries Mixed Debits and Credits. | |
| Company Name | 5 | 16 | Left-justified, alphanumeric | parms_mst.company - Form field is 60 characters, but is truncated here to 16. |
| Filler | 21 | 20 | Blanks | Not used. |
| Company ID | 41 | 10 | Left-justified, alphanumeric | apparms_mst.ach_co_id - Company number. Value is the same as Company in the file header record, unless multiple companies or divisions are sent in one transmission. |
| Entry Class | 51 | 3 | Alphabetic | Value is PPD. This identifies the entries in the class. The standard entry class used here is Prearranged Payments and Deposit entries. |
| Entry Description | 54 | 10 | Left-justified, alphanumeric | Value is Vouchers. This is a description of the transaction that may be printed on the receiver's bank statement. |
| Company Descriptive Date | 64 | 6 | MMDDYY | dbo.getsitedate. This is the current date, which is used to identify the transactions. It may be printed on the receiver's bank statement. |
| Effective Entry (Transaction) Date | 70 | 6 | YYMMDD | dbo.getsitedate. This is the current date, which is used to post the transactions. |
| Filler | 76 | 3 | Blanks | Not used. |
| Originator Status Code | 79 | 1 | Value is 1. This identifies the bank as a depository financial institution bound by the rules of the ACH. | |
| Originating ID | 80 | 8 | Fill with zeros to left | apparms_mst.ach_orig_id - The transit routing number of the originating financial institution. |
| Batch Sequence Number | 88 | 7 | Fill with zeros to left | Initial value is 1. Number batches sequentially. |
This record contains the information needed to post a deposit to an account, such as the receiver's name, account number, and payment amount.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 6. This identifies a detail entry record. | |
| Transaction Code | 2 | 2 | Numeric | Identifies the account type at the receiving financial institution as a deposit destined for a checking account. |
| Detail Transit | 4 | 8 | Fill with zeros to left | vendor_mst.transit - Transit routing number of the receiver's financial institution. |
| Check Digit | 12 | 1 | Numeric | The ninth digit of the receiving financial institution's transit routing number, calculated by SyteLine. |
| Account Number | 13 | 17 | Left-justified, alphanumeric | vendor_mst.account - Receiver's bank account number. |
| Amount | 30 | 10 | Fill with zeros to left (no decimal point) | DerDomAmtApplied * 100 - Transaction amount in dollars with two decimal places |
| Vendor ID | 40 | 15 | Left-justified, alphanumeric | vendor_mst.vend_num - This vendor number may be printed on the receiver's bank statement. |
| Vendor Name | 55 | 22 | Left-justified, alphanumeric | vendaddr_mst.name - Form field is 60 characters, but is truncated here to 22. |
| Filler | 77 | 2 | Blanks | Not used. |
| Addenda | 79 | 1 | Numeric | Value is 0 - Indicates no addenda records for this transaction. |
| Detail Orig ID | 80 | 8 | Fill with zeros to left | apparms_mst.ach_orig_id - This value is the origination ID of the receiver's bank. |
| Detail Sequence | 88 | 7 | Fill with zeros to left | Initial value is 1. This value increments for every payment record. |
NOTES:The optional
Entry Detail Addenda record is not included with SyteLine A/P EFT files.
There are line breaks (carriage return characters) between each detail
record.
This record appears at the end of eacth batch. It holds totals for the batch.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 8. This identifies a batch control total record. | |
| Service Class | 2 | 3 | Numeric | Value is 200 - Identifies the type of entries in the batch as ACH Entries Mixed Debits and Credits. |
| Entry Count | 5 | 6 | Numeric. Fill with zeros to left | Total number of detail records processed in the batch. |
| Entry Hash | 11 | 10 | Numeric | Value is calculated by SyteLine. |
| Total Debit Amount | 21 | 12 | Numeric. Fill with zeros to left | Dollar total of debit entries in the batch. |
| Total Credit Amount | 33 | 12 | Numeric. Fill with zeros to left | Sum of DerDomAmtApplied for each payment *100. This is the dollar total of credit entries in the batch. |
| Company ID | 45 | 10 | apparms_mst.ach_co_id - This should match the Company ID used in the batch header. | |
| Filler | 55 | 25 | Blanks | Not used. |
| Origination ID | 80 | 8 | Numeric. Fill with zeros to left | apparms_mst.ach_orig_id - This should be the originating bank's routing number. |
| Sequence | 88 | 7 | Numeric. Fill with zeros to left | Initial value is 1. This indicates the number of the batch associated with the control record. |
This record provides a final check on the submitted data. It contains block and batch counts and totals for each type of entry.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 9. This identifies a file control record. | |
| Batch Count | 2 | 6 | Numeric. Fill with zeros to left | Initial value is 1. This is the total number of batch header records in the file. |
| Block Count | 8 | 6 | Numeric. Fill with zeros to left | This is the total number of physical blocks in the file, including the file header and file control records. Calculated by SyteLine (blocks of 10). |
| Entry Count | 14 | 8 | Numeric. Fill with zeros to left | This is the total number of detail records in the file. |
| Entry Hash | 22 | 10 | Numeric. Fill with zeros to left | Value is calculated by SyteLine. |
| Total Debit | 32 | 12 | Numeric. Fill with zeros to left | Dollar total of debit entries in the file. |
| Total Credit | 44 | 12 | Numeric. Fill with zeros to left | Sum of DerDomAmtApplied for every payment * 100. This is the dollar total of credit entries within the file. |
| Reserved | 56 | 39 | Blanks | Leave this reserved field blank. |
IAT records are used when payments are sent to a foreign country.
This record includes your company name and company number. It also designates the immediate destination of the entries in the file.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 1. This identifies the file header record. | |
| Priority Code | 2 | 2 | Value is 01. The lower the number, the higher the processing priority. Currently, only 01 is used. | |
| Destination ID | 4 | 10 | Fill with zeros to the left | apparms_mst.ach_dest_id - Bank's transit routing number There is a space between Priority Code and Destination ID. |
| Company ID | 14 | 10 | Left-justified | apparms_mst.ach_co_id - Company number. The use of an IRS federal tax ID number is recommended. |
| Creation Date | 24 | 6 | YYMMDD | dbo.getsitedate - Date the input file was created. |
| Creation Time | 30 | 4 | HHMM | dbo.getsitedate - Time of day the input file was created. |
| File ID | 34 | 1 | Uppercase A-Z Numeric 0-9 | Initial value is A. This is a code to distinguish between multiple input files. If more than one file is delivered, they must have different file IDs. |
| Record Size | 35 | 3 | Value is 094 - Number of bytes per record. | |
| Blocking Factor | 38 | 2 | Value is 10. | |
| Format Code | 40 | 1 | Value is 1. | |
| Destination Name | 41 | 23 | Left-justified | bank_hdr_mst.name - Name of bank. Form field is 60 characters, but is truncated here to 23. |
| Company Name | 64 | 23 | Left-justified | parms_mst.company - Name of your company. Form field is 60 characters, but is truncated here to 23. |
| Return | vbNewLine or vbCLf |
NOTE: There is a space between the File Header Company Name and the Batch Header Record Code.
This record contains the effective entry (transaction) date, which is the date the deposits will be settled. The record also identifies your company and contains an entry description for debits and credits in this batch.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 5. This identifies the batch header record.
There is a space between the Company Name and the Batch Header Record Type. |
|
| Service Class | 2 | 3 | Value is 200. This identifies the type of entries in the batch as ACH Entries Mixed Debits and Credits. | |
| 5 | 16 | Blanks |
parms_mst.company - Form field is 60 characters, but is truncated here to 16. | |
| Foreign Exchange Indicator | 21 | 2 | Value is FF. There is no foreign exchange conversion for entries transmitted using this code. | |
| Foreign Exchange Reference Indicator | 23 | 1 | Value is 3. Transaction does not use foreign exchange. | |
| Foreign Exchange Reference | 24 | Space filled | ||
| ISO Destination Country Code | 39 | 2 | vendaddr_mst.country. Use ISO Country Codes. | |
| Originator ID | 41 | 10 | fill 0 to left | If a person is not originating the batch, this field must contain the IRS Taxpayer Identification number (TIN) of the originators specified in the Originator Name field. NACHA rules do not indicate whether an alpha or number prefixing the TIN is acceptable. NACHA has recommended that third-party senders initiating an IAT transaction on behalf of another part use this field for the third-party sender's TIN. |
| Entry Class | 51 | 3 | Alphabetic | Value is IAT. |
| Entry Description | 54 | 10 | Left-justified, alphanumeric | Value is Vouchers. This is a description of the transaction that may be printed on the receiver's bank statement. |
| ISO Orig Curr Code | 64 | 3 | USD | |
ISO Dest Curr Code |
67 | 3 | USD | |
| Date | 70 | 6 | MMDDYY | dbo.getsitedate |
| Settlement Date | 76 | Blank | Leave blank. | |
| Originator Status Code | 79 | 1 | Value is 1. This identifies the bank as a depository financial
institution bound by the rules of the ACH.
There are 3 spaces between the Transaction Date and the Originator Status. |
|
| Originating ID | 80 | 8 | Fill with zeros to left | apparms_mst.ach_orig_id - The transit routing number of the originating financial institution. |
| Batch Sequence Number | 88 | 7 | Fill with zeros to left | Initial value is 1. Number batches sequentially. |
| Return | vbNewLine or vbCLf |
This record contains the information needed to post a deposit to an account, such as the receiver's name, account number, and payment amount.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 6. This identifies a detail entry record. | |
| Transaction Code | 2 | 2 | Numeric | Identifies the account type at the receiving financial institution as a deposit destined for a checking account. If DerDomAmtApplied > 0 then the value is 22 or 32; otherwise it is 27 or 37, depending on whether the vendor account is checking or savings. |
| Detail Transit | 4 | 8 | Fill with zeros to left | vendor_mst.transit - Transit routing number of the receiver's financial institution. |
| Check Digit | 12 | 1 | Numeric | The ninth digit of the receiving financial institution's transit routing number, calculated by SyteLine. |
| Num Addenda Records | 13 | 4 | 7. This number represents the number of addenda records associated with each Entry Detail record. | |
| Filler | 17 | 13 | Blanks | |
| Amount | 30 | 10 | Fill with zeros to left (no decimal point) | DerDomAmtApplied * 100 - Transaction amount in dollars with two decimal places |
| Account Number | 40 |
35 |
Left-justified | vendor_mst.account - Receiver's bank account number. |
| Filler | 75 | 2 | Blanks | |
| Filler | 77 | 1 | Blanks | |
| Filler | 78 | 1 | Blanks | |
| Addenda | 79 | 1 | Numeric | Value is 1 - Indicates that addenda records exist for this transaction. |
| Trace Number | vendor_mst.transit + #. First 8 digits is vendor transit number; the last 7 digits must be incremented by 1 for each Detail record. | |||
| Detail Addenda Record Indicator | vbNewLine or vbCLf |
NOTES:The optional
Entry Detail Addenda record is not included with SyteLine
A/P EFT files.
There are line breaks (carriage return characters) between each detail
record.
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 10. | |
| Transaction Code | 4 | 3 | Value is BUS. | |
| Foreign Payment Amount | 7 | 18 | Numeric. Fill with zeros to left | DerDomAmtApplied * 100
No decimal. |
| Foreign Trace Number | 25 | 22 | Space filled | Blank |
| Receiving Company Name | 47 | 35 | vendaddr_mst.name | |
| Reserved | 82 | 6 | Space filled | |
| Entry Detail | 88 | 7 | Fill with zeros to left | This number is the same as the last seven digits of the Trace Number. |
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 11. | |
| Originator Name | 4 | 35 | parms_mst.company
Field is 60 characters but will be truncated to 35. |
|
| Street Address | 39 | 35 | parms_mst.addr##1
This is the physical address of the originator. A PO Box is not allowed. |
|
| Reserved | 74 | 14 | ||
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 12. | |
| Originator City and State | 4 | 35 | parms_mst.city + * + parms_mst.state + \
The originator's city and state/province. Use an asterisk between the city and state/province. Use a backslash as the terminator. |
|
| Originator Country and Postal Code | 39 | 35 | parms_mst.country + * + parms_mst.zip + \
The originator's country and ZIP code. Use an asterisk between the country and ZIP. Use a backslash as the terminator. |
|
| Reserved | 74 | 14 | ||
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 13. | |
| Originating Bank Name | 4 | 35 | bank_hdr_mst.name | |
| 39 | 2 | |||
Originating Bank ID |
41 | 34 | apparms_mst.ach_orig_id | |
| Originating Branch Country Code | 75 | 3 | parms_mst.country | |
| Reserved | 78 | 10 | Blank | |
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 14. | |
| Receiving Bank Name | 4 | 35 | vendor_mst.bank_name | |
| Receiving Number Qualifier | 39 | 2 | vendor.transit_reference
If US is specified for the Receiving Branch Country Code, this defaults to 01. |
|
Receiving Bank Routing Number |
41 | 34 | vendor_mst.transit | |
| Receiving Branch Country Code | 75 | 3 | vendaddr_mst.country | |
| Reserved | 78 | 10 | Blank | |
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 15. | |
| Receiver's ID Number | 4 | 15 | vendor_mst.vend_num | |
| Receiver's Street Address | 19 | 35 | vendaddr_mst.addr##1(vadRAddr_1 or VadAddr_1) | |
| Reserved | 54 | 34 | Space
filled |
|
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record contains addenda.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 7. | |
| Addenda Code | 2 | 2 | Value is 16. | |
| Receiver City and State | 4 | 35 | vendaddr_mst.city + * + vendaddr_mst.state + \
The receiver's city and state/province. Use an asterisk between the city and state/province. Use a backslash as the terminator. |
|
| Receiver Country and Postal Code | 39 | 35 | vandaddr_mst.country + * + vendaddr_mst.zip + \
The receiver's country and ZIP code. Use an asterisk between the country and ZIP. Use a backslash as the terminator. |
|
| Reserved | 74 | 14 | ||
| EntryDetailSeqNumber | 88 | 7 | ||
| Return | vbNewLine or vbCLf |
This record appears at the end of each batch. It holds totals for the batch.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 8. This identifies a batch control total record. | |
| Service Class | 2 | 3 | Numeric | Value is 200 - Identifies the type of entries in the batch as ACH Entries Mixed Debits and Credits. |
| Entry Count | 5 | 6 | Numeric. Fill with zeros to left | Total number of detail records processed in the batch. |
| Entry Hash | 11 | 10 | Numeric | Value is calculated by SyteLine. |
| Total Debit Amount | 21 | 12 | Numeric. Fill with zeros to left | Sum of all negative DerDomAmtApplied for each payment *100.. |
| Total Credit Amount | 33 | 12 | Numeric. Fill with zeros to left | Sum of all positive DerDomAmtApplied for each payment *100. This is the dollar total of credit entries in the batch. |
| Company ID | 45 | 10 | apparms_mst.ach_co_id - This should match the Company ID used in the batch header. | |
| Filler | 55 | 25 | Blanks | Not used. |
| Origination ID | 80 | 8 | Numeric. Fill with zeros to left | apparms_mst.ach_orig_id - This should be the originating bank's routing number. |
| Sequence | 88 | 7 | Numeric. Fill with zeros to left | Initial value is 1. This indicates the number of the batch associated with the control record. |
| Return | vbNewLine or vbCLf |
This record provides a final check on the submitted data. It contains block and batch counts and totals for each type of entry.
| Field Description | Position | Length | Format | SyteLine Field or Notes |
|---|---|---|---|---|
| Record Type Code | 1 | 1 | Value is 9. This identifies a file control record. | |
| Batch Count | 2 | 6 | Numeric. Fill with zeros to left | Initial value is 1. This is the total number of batch header records in the file. |
| Block Count | 8 | 6 | Numeric. Fill with zeros to left | This is the total number of physical blocks in the file, including the file header and file control records. Calculated by SyteLine (blocks of 10). |
| Entry Count | 14 | 8 | Numeric. Fill with zeros to left | This is the total number of detail and addenda records in the file. |
| Entry Hash | 22 | 10 | Numeric. Fill with zeros to left | Value is calculated by SyteLine. |
| Total Debit | 32 | 12 | Numeric. Fill with zeros to left | Sum of negative DerDomAmtApplied for every payment * 100Dollar total of debit entries in the file. |
| Total Credit | 44 | 12 | Numeric. Fill with zeros to left | Sum of positive DerDomAmtApplied for every payment * 100. This is the dollar total of credit entries within the file. |
| Reserved | 56 | 39 | Blanks | Leave this reserved field blank. |
| Return | vbNewLine or vbCLf |