To adjust a posted transaction, use the following payment adjustment process.
NOTE: You can only adjust a draft that was manually entered and not one generated from an invoice.
To create the adjustment, do the following:
NOTE: To find the check or draft number for the adjustment, you might need to review the A/R Posted Transactions Detail form.
To increase the payment amount, enter a positive number. To reduce the payment amount, enter a negative number.
The G/L Reference field displays either ARPA or ARPR and the check or draft number. The Description field displays either Payment Adj or Reapplication and the check or draft number.
NOTE:When you distribute the adjustment, you can only distribute it to either an invoice or a finance charge.
Use this report to verify that the payments and their related distributions are accurate. The Payment Type field on the report displays adjustment to indicate an adjustment.
NOTE: The system does not post transactions containing errors. If a transaction contains errors, correct the errors and perform the posting again.
The adjustment will show up as a payment on the A/R Posted Transactions Detail form.