Creating a Manual Check
- On the A/P
Payments form, select Actions > New.
- Specify information in these fields:
- Vendor - Select the number
of the vendor you are entering the manual check for.
- Payment Type - To create
a manual check, select Manual Check.
- Reapplication - If the manual
check payment is for a reapplication, select this check box.
- Check Number - Enter the
check number for the manual check you are issuing.
- Check Seq - Enter the check
sequence number, or accept the default of the next incremental
number. The system uses this number to keep the distributions
in numerical order.
- Check Date - Enter the check
date, or accept the default of today's date.
- Bank Code - This field displays
the vendor's default bank code, but you can change it to the code
of the bank from which the payment is being made (if applicable).
- Notes - (Optional) Enter
notes about the payment.
- Reference - Enter the description
that is to appear in the journals for this transaction, or accept
the default, which is the APP followed by the vendor number.
- Check Amt - Enter the amount
of the check.
- To save the payment, select Actions > Save.
- Select Distributions.
- Select Actions > New, and distribute
the payment.
- Print and post the check.
Related Topics
Accounts Payable
Steps
Generating
Automatic Payments