Creating a Standard Draft
- On the A/P
Payments form, select Actions > New.
- Specify information in these fields:
- Vendor - Select the number
of the vendor you are entering the standard draft for.
- Payment Type - Select Standard
Draft.
- Check Seq - Accept the sequence
number that displays. The system uses this number to keep the
distributions in numerical order.
- Check Date - Enter the draft
date, or accept the default, which is today's date.
- Draft Due - The default payment
due date displays, but you can change it to a different date on
which the draft is to be due.
- Bank Code - The vendor's
default bank code displays, but you can change it to the code
of the bank from which the payment is being made (if applicable).
- Notes - (Optional) Enter
notes about the payment.
- Reference - Enter a description
which is to appear in the journals for this transaction, or accept
the default, which is APP followed by the vendor number.
- To save the payment, select Actions > Save.
- Select Distributions.
- To distribute the payment, select Actions > New.
- On the General tab, in the Type field, select one
of the following options:
- Voucher - Applies the payment
to a particular voucher. Enter the voucher number in the Vch/Seq
field.
- Open - Applies the payment
to the vendor, not to a specific voucher.
- Finish distributing
the payment.
- Print and post the draft.
Related Topics
Accounts Payable
Steps
Printing
and Posting A/P Drafts