The third step in creating a Fixed Asset file is to generate a depreciation schedule. To generate a depreciation schedule:
For details about calculations performed for these depreciation methods, see About Depreciation.
NOTE: To use a custom depreciation method that you defined, you must first define it using the Fixed Asset Depreciation Tables form.
The system depreciates the asset when the Generate Depreciation activity is finished. There is no special setting for depreciating an asset for part of a year or part of a month.
For example, if an asset was purchased in July, and you want to accumulate 1/2 year of depreciation, run the Generate Depreciation utility for the months of July through December, assuming periods equal calendar months. The number of times the utility has been run is the number of months the asset is depreciated.
During depreciation generation, if a switch to the straight-line method has occurred, the Auto Crossover field is selected.
NOTE: For additional, special expensing or depreciation of an asset during its first year, enter both the Bonus Depr and Bonus Depr Code.
NOTE: The system calculates the default amount by accessing the useful life and the number of accounting periods from the General Ledger. This value does not decrease.
NOTE: If you are assigned a Thailand Localization license, the number of units to depreciate is incremented by one when the depreciation method is not USAGE and the acquisition date falls between the start and end of the specified accounting period. For example, if the depreciation frequency is set to Period (usually 12 in one year) and the acquisition date is 10-Jan-2013, then for a "Useful Life" of 5 years the number of units to depreciate is about 61 (12*5 + 1) instead of 60 (12*5). Similarly, if the acquisition date is specified to the beginning of the month (1-Jan-2013) then the number of units to depreciate is 60 (12*5).
NOTE: You must include the bonus amount in the Accum Depr and YTD Depreciation fields before generating depreciation. You must post the bonus amount manually to the General Ledger.
This field is linked to the Date to Start Depreciation field on the Fixed Assets form.
NOTE: If you want a salvage value, enter the estimated value of an asset at the end of its useful life. The system does not depreciate an asset below its salvage value.