Voiding Posted Checks
After checks have been posted, you can void them using either the A/P Payments
form or the Void
A/P Posted Payments form.
After voiding the checks, you can reprint them.
Voiding Posted Checks Using the A/P Payments Form
To void posted checks using the A/P
Payments form:
- Select Actions > New.
- Enter data in the following fields:
- Vendor - Select the number
of the vendor whose check you want to void.
- Bank Code - Enter a valid
bank code for the bank against whom the original check was issued.
- Payment Type - Select Manual
Check.
- Check Number - Enter the
number of the check you want to void.
- Check Date - Enter the date
of the manual check.
- Seq - Accept the default,
which is the next incremental number. The system uses this number
only to keep the distributions in numerical order.
- Check Amt - Enter the negative
value of the check you are voiding. For example, to void a $250.00
check, enter -250.00.
- In the G/L Reference field, enter the description for this
transaction that is to appear in the journals. The default is APP,
followed by the vendor number.
- Select Distributions.
- Select Actions > New.
- Distribute to the vouchers as negative amounts.
- Print the final register and post the negative check.
NOTE: The check number that defaults
on the A/P Check Printing and Posting form during this
process is strictly for standard checks. You do not need to update
this number when posting the negative manual check.
Voiding a Check Using the Void A/P Posted Payments Utility
NOTE: If the A/P
payments are manual checks, are compressed, or are multi-site, you cannot
void them using this utility.
To void a payment using the Void
A/P Posted Payments utility:
- Enter data in the following fields:
- Select Process.
Related Topics
Accounts Payable
Steps
Posting Vouchers
- Detail
Printing
and Posting Checks