Entering Information About a New Employee
To add a new employee record to the system, use the Employees
form.
- On the main toolbar, click the Filter-in-Place button.
- To create a new record, select Actions > New. The system
opens the Copy From Applicant (Modal) form.
- (Optional) Perform one of the following actions:
- In the Employee field:
- If you want the system to assign the next available employee
ID, leave it blank.
- If you want to manually assign a custom ID, enter the identifier.
- Enter information for the employee in all the required fields.
Required fields include:
- Shift - Select the shift
to which the new employee is assigned.
- Wage Acct - Select the account
from which the employee's earnings are to be paid.
- Emp Type - Select the employment
payment type for the new employee. This indicates whether the
employee is to be paid on an hourly basis, a salaried basis, or
some other basis.
- Pay Freq - Select the frequency
at which the employee is to be paid.
- Generate Payroll From - Select
the payroll basis on which the employee's pay is to be calculated.
- Marital Status - Select the
employee's marital status to be used for the employee's federal
income tax filing status.
- (Optional, but recommended) Enter any other information available
about the new employee. At the least, you should have the employee's
Social Security Account Number (SSN), for tax purposes.
For more information about other fields on this form, see the appropriate
field help topics.
Related Topics
Human Resources
Overview
Setting
Up Employee Deductions and Earnings
Setting
Up an Employee for Direct Deposit
Steps for Setting
Up Employees
Viewing,
Adding, and Changing Employee Information